i. MX8M Nano: Camera App crash issue on Android 11.0.0_2.4.0 (kernel 5.10.52) .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i. MX8M Nano: Camera App crash issue on Android 11.0.0_2.4.0 (kernel 5.10.52) .

4,098 Views
oferausterlitz
Senior Contributor II

Steps to repo.

Launch Camera App from android and click a picture.

After clicking observe Camera app. closes and on logcat spew crash is observed.

Camera recording works fine.

 

Attaching logcat o/p from the crashes.

 

cheers,

mohit

Labels (1)
0 Kudos
Reply
13 Replies

3,869 Views
oferausterlitz
Senior Contributor II

@joanxie I debugged a little more and if I limit the resolution to 720p(see below) in the camera HAL, it no longer crashes.

 

--- a/camera/ISPCameraDeviceHWLImpl.cpp
+++ b/camera/ISPCameraDeviceHWLImpl.cpp
@@ -87,7 +87,7 @@ status_t ISPCameraDeviceHwlImpl::initSensorStaticData()
         w_min, w_max, w_step, h_min, h_max, h_step);
 
     // Support resolutions requeted by CCD
-    uint32_t ispResCandidate[] = {176, 144, 320, 240, 640, 480, 1280, 720, 1920, 1080, 3840, 2160};
+    uint32_t ispResCandidate[] = {176, 144, 320, 240, 640, 480, 1280, 720};
     uint32_t ispResCandidateNum = ARRAY_SIZE(ispResCandidate)/2;
     uint32_t ispRes[MAX_RESOLUTION_SIZE];

     uint32_t ispResNum = 0;

 

cheers,

mohit

0 Kudos
Reply

3,879 Views
oferausterlitz
Senior Contributor II

@joanxie I don't have NXP imx8mn ddr4 device with me. I have moved to Android 11.0.0_2.6.0 (Linux 5.10.72 kernel) and observed the same crash. Please see camera_crash_Android_11.0.0_2.6.0.txt.

For me, the crash comes on the first try itself.

The camera name is already there in the log "isi-capture 32e20000.isi:cap_device: mxc_isi_capture_open: src name is ov5640 1-003c"

After the crash, I can still open the app and can see the preview, click the picture which results in the crash.

 

cheers,

mohit

0 Kudos
Reply

3,863 Views
joanxie
NXP TechSupport
NXP TechSupport

After the crash, I can still open the app and can see the preview, click the picture which results in the crash.

>what crash do you mean? the camera is frozen? could you borrow a ddr4 board from local DFAE? the expert team couldn't reproduce this issue either, my test steps is:

1) open the camera app

2) click the picture to save picture more than 10 pictures

3) open all of the pictures to review one by one, the app or the display aren't frozen

when I take picture, I can get the message from display:

[ 123.046711][ T466] bypass csc
[ 123.049836][ T466] input fmt YUV4
[ 123.053257][ T466] output fmt YUYV
[ 129.277557][ T349] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400000 fc=4000000 cc=32 chg=a
[ 159.215704][ T466] bypass csc
[ 159.218786][ T466] input fmt YUV4
[ 159.222203][ T466] output fmt YUYV
[ 161.227841][ T1772] bypass csc
[ 161.230986][ T1772] input fmt YUV4
[ 161.234419][ T1772] output fmt YUYV
[ 162.575045][ T465] bypass csc
[ 162.578415][ T465] input fmt YUV4
[ 162.582228][ T465] output fmt YUYV
[ 164.511270][ T466] bypass csc
[ 164.514369][ T466] input fmt YUV4
[ 164.517800][ T466] output fmt YUYV
[ 165.375910][ T465] bypass csc
[ 165.379013][ T465] input fmt YUV4
[ 165.382456][ T465] output fmt YUYV
[ 167.279484][ T466] bypass csc
[ 167.282583][ T466] input fmt YUV4
[ 167.286014][ T466] output fmt YUYV

 

if you need further test on imx8mm board, pls let me know it, we need reproduce this on nxp imx8mm board

 

0 Kudos
Reply

3,850 Views
oferausterlitz
Senior Contributor II

@joanxie 

>>what crash do you mean?

I am not sure if you got the chance to look at the logs I attached earlier. I am pasting the some part of it here.

--------- beginning of crash
libc    : Fatal signal 11 (SIGSEGV), code 2 (SEGV_ACCERR), fault addr 0x6dfc1f9000 in tid 1796 (Thread-2), pid 1713 (android.camera2)
I crash_dump64: obtaining output fd from tombstoned, type: kDebuggerdTombstone
I tombstoned: received crash request for pid 1796
I crash_dump64: performing dump of process 1713 (target tid = 1796)
: *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
: Build fingerprint: 'Android/som_mx8mn/som_mx8mn:11/RQ3A.211001.001/eng.mohit.20220117.111624:userdebug/dev-keys'
: Revision: '0'
: ABI: 'arm64'
: Timestamp: 2022-01-17 21:06:26+0000
: pid: 1713, tid: 1796, name: Thread-2  >>> com.android.camera2 <<<
: uid: 10103
: signal 11 (SIGSEGV), code 2 (SEGV_ACCERR), fault addr 0x6dfc1f9000
:     x0  0000000076ae400c  x1  0000006dfc1f8fb4  x2  000000000004b8b8  x3  0000000076ee3fc0
:     x4  0000006dfc2448bc  x5  0000000076f2f8c8  x6  7190e4201c50953c  x7  f9d4633e700e82d0
:     x8  e69ef5f449f5896f  x9  0a3914222bc94bd9  x10 79f9410e68031fab  x11 d562169c6c850ada

>>the camera is frozen? 

App closes on its own after above crash, however I can re-open it and try to take the pic and it again results in the above mentioned behaviour.

 

Are you testing on imx8mm ? I have reported the issue on i. MX8M Nano. 

imx8mm does __not__ have this issue when I tested it on Android 11.0.0_2.4.0 (kernel 5.10.52).

Also please note "if I limit the resolution to 720p(see below) in the camera HAL, it no longer crashes."

cheers,

mohit

0 Kudos
Reply

3,713 Views
joanxie
NXP TechSupport
NXP TechSupport

 how about the status now? the expert team couldn't reproduce this, if you still need help, pls answer these questions from expert team:

“Did the customer modify the code base at all around the cameras? Are they using a custom Android build? If so, can they share those code changes so we can reproduce the bug on our end? It will be much easier to debug if I can reproduce the issue here.

If not, I can try and send this to the rest of the video team to see if anyone has seen an error like this before.”

 

0 Kudos
Reply

3,701 Views
oferausterlitz
Senior Contributor II

Yes, the issue is still present. As a work around I have capped the resolution to 720p. However, we still need a fix for it.

 

 

cheers,

mohit

0 Kudos
Reply

3,697 Views
joanxie
NXP TechSupport
NXP TechSupport

if you still have issue, do you mind answering the below question from expert team?

“Did the customer modify the code base at all around the cameras? Are they using a custom Android build? If so, can they share those code changes so we can reproduce the bug on our end? It will be much easier to debug if I can reproduce the issue here.

If not, I can try and send this to the rest of the video team to see if anyone has seen an error like this before.”

 

0 Kudos
Reply

3,839 Views
joanxie
NXP TechSupport
NXP TechSupport

sorry, this is my typo, I tested on imx8mn ddr4 board of course, I will forward your message to expert team and discussed with them, but I still suggest that you can test on nxp board if you could borrow this from local DFAE

0 Kudos
Reply

3,800 Views
oferausterlitz
Senior Contributor II

@joanxie  ANy update?

Tags (1)
0 Kudos
Reply

4,005 Views
oferausterlitz
Senior Contributor II

Hi Joanxie,

    We are using DDR4 based VAR-SOM-MX8M-NANO and the issue is 100% repro. with Android 11.0.0_2.4.0 (kernel 5.10.52) and works fine with Android 11.0.0_1.0.0 (kernel 5.4.47).

 

cheers,

mohit

0 Kudos
Reply

3,953 Views
joanxie
NXP TechSupport
NXP TechSupport

I have downloaded the new android bsp from official website and flashed to my imx8mn ddr4 board again, I found my camera app is find with capturing picture, do you have nxp imx8mn ddr4 board to test? I couldn't reproduce this on my board right now,I launched the app and took picture more than 10 times, what camera do you use? I used ov5640, after you get the crash issue, could you open the app again?

0 Kudos
Reply

3,976 Views
joanxie
NXP TechSupport
NXP TechSupport

my camera app has different issue on nxp imx8mn ddr4 board, we already escalated this issue to the internal team, pls wait for further debug

0 Kudos
Reply

4,025 Views
joanxie
NXP TechSupport
NXP TechSupport

what board do you test? I have tested on my imx8mn lpdd4 board without issue, I open the camera app, and capture almost 10 pictures, and close the app or ctrl+c on the console, don't find any crash issues