i.MX8M Mini Uboot while loading it shows invalid partition 1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Mini Uboot while loading it shows invalid partition 1

790 Views
Hariharan1
Contributor III

BuildInfo:
- ATF 70fa7bc
- U-Boot 2019.04-04771-g4d377539a1

Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Run CMD11 1.8V switch
Net:
Warning: ethernet@30be0000 using MAC address from ROM
eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
Run CMD11 1.8V switch
** Invalid partition 1 **
** Invalid partition 1 **
Booting from net ...

 

anyone suggest your thoughts. How do i resolve this error?

Labels (1)
0 Kudos
Reply
1 Reply

755 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Make sure that you burn ok your board, since this erros is due to a miss of rootfs or kernel, you can view the step by step on:

https://www.nxp.com.cn/docs/en/quick-reference-guide/8MMINIEVKQSG.pdf

 

Regards

 

0 Kudos
Reply