i.MX8M Mini Uart丢包

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Mini Uart丢包

657 Views
lizboxy
Contributor I

我们使用i.MX8M mini,遇到如下问题,能否帮我们分析一下原因:

问题描述:

    uart配置:如图片       

    问题现象:

    使用uart3(直接将imx8mmuart3飞线出来连接PCusbuart模块),PC使用115200波特率发送大小为177字节的数据至imx8mm-uart3microcom -s 115200 /dev/ttxmxc2),imx8mm收到会丢包。

    imx8mm的波特率改为2000000microcom -s 2000000 /dev/ttxmxc2),PC发送大小为177字节至imx8mm-uart3imx8mm-uart3同样会丢包。 

丢包情况说明:

2000000波特率 8-90%会丢

115200 数据大了后 比如100多个字节  40%的概率丢

imx8m-mini uart3所接设备没有CTS/RTS,我们测试发现在2M波特率的情况下,刚好32字节数据测试10小时,未发现丢包;超过32字节8~90%的概率丢包,数据上百字节99.9%概率丢包

Labels (1)
Tags (1)
0 Kudos
1 Reply

577 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which version of BSP(Linux?) are you using?

Could you show me how you connect the UART signals? (TX,RX,GND)?

0 Kudos