i.MX8M Mini - USB isochronous transfer fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Mini - USB isochronous transfer fail

150 Views
Jamie01
Contributor I

Hi,

We cannot get the following USB camera to work and start streaming.

libuvc calls "libusb_submit_transfer fail return -1". This is USB isochronous transfer failing. It failed when uvc_stream_start USB was transferring.

It seems the issue could be related to i.MX8M Mini USB full speed. We tested the same camera sample on the other board with i.MX8M Plus CPU. It works out normally. 

Please help to solve this issue. 

 

Please find the following link for the camera specs: 

PureThermal 2

https://groupgets-files.s3.amazonaws.com/PT2/PureThermal%202%20-%20Datasheet%20-%201.7.pdf

Lepton_Series

https://groupgets-files.s3.amazonaws.com/lepton/Resources/Lepton%20Series%20Datasheet.pdf

 

0 Kudos
Reply
2 Replies

107 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

Which board are you using?

0 Kudos
Reply

146 Views
Jamie01
Contributor I
By the way, it shows "[ 940.873815] usb 1-1: usbfs: usb_submit_urb returned -28"
From kernel's USB driver error log
0 Kudos
Reply