i.MX8M Mini Brownout Power Sequencing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Mini Brownout Power Sequencing

ソリューションへジャンプ
1,301件の閲覧回数
kevinl
Contributor II

Hello,

For our design we are considering brownout condition where voltage on PMIC input drops below UVLO before the complete power down sequence is completed.

For the shutdown part, this seems to be OK based on Table 18 which shows they all just need to be disabled at the same time.

However, if the PMIC input voltage comes back quickly, the power up sequence may start before all rails have discharged to 0V. Does this violate the datasheet? Do I need to add a delay to the PMIC enable to allow for all rails to fully discharge? If so, to what voltage?

0 件の賞賛
返信
1 解決策
1,296件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

 

>power up sequence may start before all rails have discharged to 0V.

>Does this violate the datasheet?

 

yes violate.

 

>Do I need to add a delay to the PMIC enable to allow for all rails to fully discharge?

 

yes

 

>If so, to what voltage?

 

as estimation one can consider "VIL" from Table 21. GPIO DC parameters

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,297件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

 

>power up sequence may start before all rails have discharged to 0V.

>Does this violate the datasheet?

 

yes violate.

 

>Do I need to add a delay to the PMIC enable to allow for all rails to fully discharge?

 

yes

 

>If so, to what voltage?

 

as estimation one can consider "VIL" from Table 21. GPIO DC parameters

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

 

Best regards
igor

0 件の賞賛
返信