i.MX8M MINI on Chromium

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M MINI on Chromium

321 Views
rizwanm
Contributor II

Hi Team,

Unable to play .mp4 video offline in i.MX8M MINI Custom board in Linux 5.4.70 version 

(Chromium 83.0.4103.116 stable)

iMX8M Mini, using Zeus 5.4.47

Is it possible to play media formats AAC, MP3, and H.264 ? in i.MX8M MINI Processor & what are all the features covers in  Chromium 83.0.4103.116 stable version

Thanks 

 

Labels (1)
0 Kudos
1 Reply

313 Views
joanxie
NXP TechSupport
NXP TechSupport

chromium issue where it tries to use the native picker dialog. which is being discussed in the community.

https://bugs.chromium.org/p/chromium/issues/detail?id=963419
https://bugreports.qt.io/browse/QTBUG-92519

The current workaround is to add gtk to the yocto image will help. Also there is fix in the above thread, which you can point to customer to adopt.

 

 

0 Kudos