Hi Team,
Unable to play .mp4 video offline in i.MX8M MINI Custom board in Linux 5.4.70 version
(Chromium 83.0.4103.116 stable)
iMX8M Mini, using Zeus 5.4.47
Is it possible to play media formats AAC, MP3, and H.264 ? in i.MX8M MINI Processor & what are all the features covers in Chromium 83.0.4103.116 stable version
Thanks
chromium issue where it tries to use the native picker dialog. which is being discussed in the community.
https://bugs.chromium.org/p/chromium/issues/detail?id=963419
https://bugreports.qt.io/browse/QTBUG-92519
The current workaround is to add gtk to the yocto image will help. Also there is fix in the above thread, which you can point to customer to adopt.