i.MX8M-EVK Touch support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M-EVK Touch support

Jump to solution
2,028 Views
ko-hey
Senior Contributor II

Hi all

 

I have a question about touch support for i.MX8M-evk.

 

According to the following release note, i.MX8M Mini supports touch.

 

imx-yocto-L4.14.62_1.0.0_beta  i.MX_Linux_Release_Notes.pdf

Features on i.MX 8M Mini: Supports OLED MIPI panel and touch.

https://www.nxp.com/pages/alpha-beta-bsps-for-microprocessors:IMXPRERELEASES

 

Will i.MX8M also support touch in L4.14.62_1.0.0 ?

 

Ko-hey

 

0 Kudos
Reply
1 Solution
1,620 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, of course, imx8M supports MX8-DSI-OLED which  is a MIPI-DSI interface for OLED display with touch screen support

View solution in original post

0 Kudos
Reply
3 Replies
1,621 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, of course, imx8M supports MX8-DSI-OLED which  is a MIPI-DSI interface for OLED display with touch screen support

0 Kudos
Reply
1,620 Views
geser_u
Contributor I

Hi,

I try to use the MX8-DSI-OLED with Android image O8.1.0_1.3.0_ANDROID_DEMO_8MQ_GA, but the touch doesn't work.

Is a configuration reqired?
Any ideas?

Urs

0 Kudos
Reply
1,620 Views
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the link as below, to add into the configure file

https://community.nxp.com/message/1035638?commentID=1035638#comment-1035638 

0 Kudos
Reply