i.MX8M-EVK Touch support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8M-EVK Touch support

跳至解决方案
1,686 次查看
ko-hey
Senior Contributor II

Hi all

 

I have a question about touch support for i.MX8M-evk.

 

According to the following release note, i.MX8M Mini supports touch.

 

imx-yocto-L4.14.62_1.0.0_beta  i.MX_Linux_Release_Notes.pdf

Features on i.MX 8M Mini: Supports OLED MIPI panel and touch.

https://www.nxp.com/pages/alpha-beta-bsps-for-microprocessors:IMXPRERELEASES

 

Will i.MX8M also support touch in L4.14.62_1.0.0 ?

 

Ko-hey

 

0 项奖励
1 解答
1,278 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes, of course, imx8M supports MX8-DSI-OLED which  is a MIPI-DSI interface for OLED display with touch screen support

在原帖中查看解决方案

0 项奖励
3 回复数
1,279 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes, of course, imx8M supports MX8-DSI-OLED which  is a MIPI-DSI interface for OLED display with touch screen support

0 项奖励
1,278 次查看
geser_u
Contributor I

Hi,

I try to use the MX8-DSI-OLED with Android image O8.1.0_1.3.0_ANDROID_DEMO_8MQ_GA, but the touch doesn't work.

Is a configuration reqired?
Any ideas?

Urs

0 项奖励
1,278 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the link as below, to add into the configure file

https://community.nxp.com/message/1035638?commentID=1035638#comment-1035638 

0 项奖励