Hi all
I have a question about touch support for i.MX8M-evk.
According to the following release note, i.MX8M Mini supports touch.
imx-yocto-L4.14.62_1.0.0_beta i.MX_Linux_Release_Notes.pdf
Features on i.MX 8M Mini: Supports OLED MIPI panel and touch.
https://www.nxp.com/pages/alpha-beta-bsps-for-microprocessors:IMXPRERELEASES
Will i.MX8M also support touch in L4.14.62_1.0.0 ?
Ko-hey
解決済! 解決策の投稿を見る。
yes, of course, imx8M supports MX8-DSI-OLED which is a MIPI-DSI interface for OLED display with touch screen support
yes, of course, imx8M supports MX8-DSI-OLED which is a MIPI-DSI interface for OLED display with touch screen support
Hi,
I try to use the MX8-DSI-OLED with Android image O8.1.0_1.3.0_ANDROID_DEMO_8MQ_GA, but the touch doesn't work.
Is a configuration reqired?
Any ideas?
Urs
you can refer to the link as below, to add into the configure file
https://community.nxp.com/message/1035638?commentID=1035638#comment-1035638