Hello,
We have purchased NXP MIPI-CSI camera MINISASTOCSI kit and followed the instructions in this application note https://www.nxp.com/docs/en/application-note/AN12187.pdf to test the camera on NXP i.MX8M EVK rev B3 running L4.9.51-ga Linux BSP release. Both camera connectors were tested. The camera output was sent to HDMI display. The frame rate we've received is around 7fps, even in lowest resolution. What should be done to get the maximum frame rates advertised by the application note above (e.g. 30fps at 1080p).
Thanks.
Felix.
HI, Tom zheng
thanks for your patch you provide, it work very well now.
if use 640*480 resolution to take video of moving object, recorded video is very clear and the video quality is good.
if use 1280*720(or 1920*1024) to take video of moving object, video is very blur and the video quality isn't good.
is it be affected by no vpu in i.MX8M EVK?
How do I solve it?
thanks a lot
I meet a similiar problem:
We have purchased NXP MIPI-CSI Ov5640 camera,
and we do camera test on NXP i.MX8M EVK, The camera output was sent to HDMI display.
when we preview and take video on ov5640, and take video of moving objects, video is very blur.
from kernel logs to see , there is many RX fifo overflow, it make some captured Frames by camera lost.
[ 867.956960] mx6s-csi 30a90000.csi1_bridge: mx6s_csi_irq_handler Rx fifo overf
low
[ 870.956451] mx6s-csi 30a90000.csi1_bridge: mx6s_csi_irq_handler Rx fifo overf
low
[ 874.273032] mx6s-csi 30a90000.csi1_bridge: mx6s_csi_irq_handler Rx fifo overf
low
"rx fifo over flow" is another topic.
If you can, please carefully apply another two packages patches.
One package(tuning.7z) include ATF, u-Boot, Kernel patches for DDR.
Another package(Camera.tar.bz2) include CSI driver patches.
Two packages must be applied on GA release for this problem.
If you still meet the "rx fifo over flow" after those packages merged, please tell us how to repeat it and show us the log info.
Thanks!
Hi Tom,
I am facing same "rx fifo overflow" error with MINISASTOCSI camera. I am trying to apply attached patches but its failing. I am using
kernel 4.19.35
u-boot-imx-2019.04
Does these patches will work with these system configuration on imx8mq-evk target?
Thanks & Regards,
Vipul Kumar
Hello Tom,
thank you for providing these patches. We have a similar problem. We get FIFO_RX_overflow error too. But only when we have high cpu usage at the same time. So thats why your "tuning" patches seem perfect. But they do not fit my version. I am running 4.14.78. On which GA version are the patches made for?
Hi Tom,
The recommended workaround for this erratum is to avoid MIPI CSI overflow happen. Two undocumented debug registers can be used to monitor CSI FIFO levels in real time. When FIFO reaches one threshold, disable CSI and restart CSI.
For example, create one program on M4 core to monitor CSI FIFO level and do as follows:
Hi, Weiping
We use I.MX8MQ and have two CSI input to capture video in (use LT6911C , two HDMI in to two LT6911C CSI output to I.MX8MQ). input video format is 1080P, 30FPS. Android 11 OS. Then display from I.MX8MQ DSI port into LCM panel.
And by current test result.
1.MIPI-CSI#1 seems ok, can display over two hours.
2.MIPI-CSI#2 is NG, around several minutes happens RX FIFO overflow.
Would like to know is there any difference in HW path/architecture, or SW (resource allocation) between MIPI-CSI#1 and MIPI-CSI#2.
Many thanks.
Martin
hi Felix:
Please check FPS by below command:
gst-launch-1.0 v4l2src ! video/x-raw,width=1920,height=1080 ! fpsdisplaysink
And please enable dma-coherent in fsl-imx8mq.dtsi for csix_bridge:
csi1_bridge: csi1_bridge@30a90000 {
compatible = "fsl,imx8mq-csi", "fsl,imx6s-csi";
reg = <0x0 0x30a90000 0x0 0x10000>;
interrupts = <GIC_SPI 42 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_DUMMY>,
<&clk IMX8MQ_CLK_CSI1_ROOT>,
<&clk IMX8MQ_CLK_DUMMY>;
clock-names = "disp-axi", "csi_mclk", "disp_dcic";
dma-coherent;
status = "disabled";
};
csi2_bridge: csi2_bridge@30b80000 {
compatible = "fsl,imx8mq-csi", "fsl,imx6s-csi";
reg = <0x0 0x30b80000 0x0 0x10000>;
interrupts = <GIC_SPI 43 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_DUMMY>,
<&clk IMX8MQ_CLK_CSI2_ROOT>,
<&clk IMX8MQ_CLK_DUMMY>;
clock-names = "disp-axi", "csi_mclk", "disp_dcic";
dma-coherent;
status = "disabled";
};
Hi Tom,
After adding dma-coherent property we get about 30fps at 1080p, which is great. We've also tested maximum resolution, 2592x1944 and received the following error:
0:00:00.643195654 510 0xff16ca0 ERROR v4l2bufferpool gstv4l2bufferpool.c:854:gst_v4l2_buffer_pool_start:<v4l2src0:pool:src> we received 6 buffer from device '/dev/video0', we want at least 7
With DMA coherency enabled, is it necessary to increase GST_V4L2_MIN_BUFFERS to 7 ? Can this parameter be modified at run-time instead of compile-time ?
Thanks a lot.
Felix.