i.MX8M EVK MIPI CSI Camera Frame Rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M EVK MIPI CSI Camera Frame Rate

28,908件の閲覧回数
felixradensky
Contributor IV

Hello,

We have purchased NXP MIPI-CSI camera MINISASTOCSI kit and followed the instructions in this application note https://www.nxp.com/docs/en/application-note/AN12187.pdf  to test the camera on NXP i.MX8M EVK rev B3 running L4.9.51-ga Linux BSP release. Both camera connectors were tested. The camera output was sent to HDMI display. The frame rate we've received is around 7fps, even in lowest resolution. What should be done to get the maximum frame rates advertised by the application note above (e.g. 30fps at 1080p).

Thanks.

Felix.

ラベル(2)
26 返答(返信)

7,538件の閲覧回数
haidong_zheng
NXP Employee
NXP Employee

hi Felix:

You can decrease GST_V4L2_MIN_BUFFERS  or increase MAX_VIDEO_MEM in drivers/media/platform/mxc/capture/mx6s_capture.c to enable camera resolution 2592x1944 preview work, but this resolution performance is not good, that is about 8 FPS.  I will check this. 

 

0 件の賞賛
返信

2,425件の閲覧回数
haidong_zheng
NXP Employee
NXP Employee

hi Felix:

Please use new 2592x1944 setting, the MAX FPS supported by OV5640 is 15FPS. 

static struct reg_value ov5640_setting_15fps_QSXGA_2592_1944[] = {
{0x3008, 0x42, 0, 0},
{0x4202, 0x0f, 0, 0}, /* stream off the sensor */
{0x3820, 0x40, 0, 0}, {0x3821, 0x06, 0, 0}, /*disable flip*/
{0x3035, 0x21, 0, 0}, {0x3036, 0xA8, 0, 0}, {0x3c07, 0x08, 0, 0},
{0x3c09, 0x1c, 0, 0}, {0x3c0a, 0x9c, 0, 0}, {0x3c0b, 0x40, 0, 0},
{0x3820, 0x40, 0, 0}, {0x3821, 0x06, 0, 0}, {0x3814, 0x11, 0, 0},
{0x3815, 0x11, 0, 0}, {0x3800, 0x00, 0, 0}, {0x3801, 0x00, 0, 0},
{0x3802, 0x00, 0, 0}, {0x3803, 0x00, 0, 0}, {0x3804, 0x0a, 0, 0},
{0x3805, 0x3f, 0, 0}, {0x3806, 0x07, 0, 0}, {0x3807, 0x9f, 0, 0},
{0x3808, 0x0a, 0, 0}, {0x3809, 0x20, 0, 0}, {0x380a, 0x07, 0, 0},
{0x380b, 0x98, 0, 0}, {0x380c, 0x0b, 0, 0}, {0x380d, 0x1c, 0, 0},
{0x380e, 0x07, 0, 0}, {0x380f, 0xb0, 0, 0}, {0x3810, 0x00, 0, 0},
{0x3811, 0x10, 0, 0}, {0x3812, 0x00, 0, 0}, {0x3813, 0x04, 0, 0},
{0x3618, 0x04, 0, 0}, {0x3612, 0x2b, 0, 0}, {0x3708, 0x21, 0, 0},
{0x3709, 0x12, 0, 0}, {0x370c, 0x00, 0, 0}, {0x3a02, 0x03, 0, 0},
{0x3a03, 0xd8, 0, 0}, {0x3a08, 0x01, 0, 0}, {0x3a09, 0x27, 0, 0},
{0x3a0a, 0x00, 0, 0}, {0x3a0b, 0xf6, 0, 0}, {0x3a0e, 0x03, 0, 0},
{0x3a0d, 0x04, 0, 0}, {0x3a14, 0x03, 0, 0}, {0x3a15, 0xd8, 0, 0},
{0x4001, 0x02, 0, 0}, {0x4004, 0x06, 0, 0}, {0x4713, 0x02, 0, 0},
{0x4407, 0x0c, 0, 0}, {0x460b, 0x35, 0, 0}, {0x460c, 0x22, 0, 0},
{0x3824, 0x01, 0, 0}, {0x5001, 0x83, 0, 70}, {0x3008, 0x02, 0, 0},
{0x4202, 0x00, 0, 0}, /* stream on the sensor */
};

2,425件の閲覧回数
oferausterlitz
Senior Contributor II

Hi Tom,

With new 2592x1944 settings and GST_V4L2_MIN_BUFFERS=6 the capture at maximum resolution works at 15fps. All other resolutions work at 30fps.

Thanks a lot for your help.

Felix.

0 件の賞賛
返信

2,425件の閲覧回数
lily_zhang
NXP Employee
NXP Employee

Hello, Felix:

We will check further and feedback to you.

gogoer‌, FYI.

0 件の賞賛
返信

2,425件の閲覧回数
lily_zhang
NXP Employee
NXP Employee

Hello, Felix:

Please check 2 changes:

- Please apply for tuning patches sent by email for eMMC test..

- Please enlarge GST_V4L2_MIN_BUFFERS in the following file from 2 to 7

/gstreamer1.0-plugins-good/1.12.2-r0/git/sys/v4l2/gstv4l2object.h  : 

#define GST_V4L2_MIN_BUFFERS 7

I will check whether more changes are required tomorrow.

2,425件の閲覧回数
ryandeville2
NXP Employee
NXP Employee

Hello xiaoli.zhang,

How vital are the tuning patches to the eMMC for streaming to disk (or rather NVM)?  We can get 30fps 1080p through two cameras to /tmp, but not to SD/eMMC.

Ryan

0 件の賞賛
返信