i.MX8DualxPlus/i.MX8QuadxPlus LPDDR4 part compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8DualxPlus/i.MX8QuadxPlus LPDDR4 part compatibility

738 Views
bimal
Contributor III

HI,

We are designing an custom board based on i.MX8DXPlus/ i.MX8QXPlus where i wanted to check the compatibility of LPDDR4 part#.

1) i.MX8QxPlus MEK board uses LPDDR4 part# MT53B768M32D4DT-062 AIT:B,

which as configuration as: No of channel 2 with 2 Chip select per channel.

2) We are using LPDDR4 part#IS46LQ32256A-062BLA3 from Mfg# ISSI,

which as configuration as: No of channel 2 with 1 Chip select per channel. Also below are the address table for ISSI part#.

pastedImage_1.png

Will it be an issue considering ISSI has single chipselect per channel? Below is the LPDDR4 schematic page attached for your reference.

Let us know your feedback for the same.

1 Reply

679 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bimal

memories with 1 chip select per channel (single rank) are also supported 

and you can use attached schematic.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------