Hello,
I started bitbake for the Yocto Scarthgap version. I added the meta-opendds layer to my distro.
I clone the layer from the OpenDDS added the layer to my bblayers.conf file.
I added OpenDDS to my local.conf file as "IMAGE_INSTALL:append = "opendds"
However, when I start bitbake, I get the following errors in the opendds-3.29.1-r0 do_package step.
After this error, the yocto image is created but none of the subscriber or publisher example applications in opendds are added to my rootfs.
Error Logs:
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libTAO_Valuetype.so.2.5.21: opendds-dev, opendds (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/tests/DCPS/FindTopic/findtopic)
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libOpenDDS_Dcps.so.3.29.1: opendds, opendds-dev (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/tests/DCPS/FooType/libDcpsFooType.so.3.29.1)
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libTAO_Valuetype.so.2.5.21: opendds-dev, opendds (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/tests/security/IDL_Serialization/Security_IDL_Serialization)
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libACE.so.6.5.21: opendds, opendds-dev (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/ACE_wrappers/TAO/tao/PI/libTAO_PI.so.2.5.21)
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libOpenDDS_Rtps.so.3.29.1: opendds, opendds-dev (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/tests/DCPS/RtpsDurableReplay/publisher)
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libTAO_PortableServer.so.2.5.21: opendds, opendds-dev (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/ACE_wrappers/TAO/orbsvcs/ImplRepo_Service/tao_imr)
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libOpenDDS_Dcps.so.3.29.1: opendds, opendds-dev (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/tests/DCPS/Reliability/IDL/libReliability.so.3.29.1)
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libOpenDDS_Dcps.so.3.29.1: opendds, opendds-dev (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/tests/DCPS/Prst_delayed_subscriber/publisher)
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libOpenDDS_Dcps.so.3.29.1: opendds, opendds-dev (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/tests/security/ConcurrentAuthLimit/ConcurrentAuthLimit)
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libACE.so.6.5.21: opendds, opendds-dev (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/tests/DCPS/KeyTest/IsBounded)
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libTAO.so.2.5.21: opendds, opendds-dev (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/tests/FACE/CallbackAndReceive/Publisher/publisher)
ERROR: opendds-3.29.1-r0 do_package: opendds-dev: Multiple shlib providers for libACE.so.6.5.21: opendds, opendds-dev (used by files: /home/yocto/yocto-nxp/build-nxp/tmp/work/armv8a-poky-linux/opendds/3.29.1/packages-split/opendds-dev/usr/share/DDS_ROOT/tests/DCPS/LivelinessTimeout/publisher)
Could you please help me these errors?
Best regards.