Hello,
I am working with an i.MX8 and I want to know the transient overshoot and undershoot at IO pin.
In the datasheet only static values are defined, which are -0.3V and VDD + 0,3V
For example Texas defines theses overshoot and undershoot like this.
Thanks and regards
Hello
I know what DS says but I am not asking for static values but dynamic ones. It is not the same.
What about if there is -0.31V during 1ps? Will i.MX8 break?
Regards
which imx8 processor do you use? imx8qm?
I checked the data sheet, nxp doesn't offer the overshoot and undershoot as percentage like TI, refer to the data sheet, the minimum allowed undershoot is -0.3V and the maximum allowed overshoot is VDD+0.3V, this is 3.3v+0.3V=3.6v for 3.3v level signal
My reply is being deleted, why?
not receive any reply, you can post again
Hello,
-0.31V during 1ps will damage i.MX8?
Regards
Hello, Yes, I know what DS says but I'm not asking for static values but dynamic ones. It is not the same. What about if there is -0.31V for 1ps? will i.MX8 break? Regards
Hello,
Yes, I know what DS says but I'm not asking for static values but dynamic ones. It is not the same.
What about if there is -0.31V for 1ps? will i.MX8 break?
Regards
Hello,
Yes, I know what DS says but I'm not asking for static values but dynamic ones. It is not the same.
What about if there is -0.31V for 1ps? will i.MX8 break?
Regards