i.MX8 overshoot and undershoot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8 overshoot and undershoot

1,201 次查看
Lubeiro
Contributor I

Hello,

I am working with an i.MX8 and I want to know the transient overshoot and undershoot at IO pin.

In the datasheet only static values are defined, which are -0.3V and VDD + 0,3V

Lubeiro_0-1747982161400.png

For example Texas defines theses overshoot and undershoot like this.

Lubeiro_1-1747982229679.png

 

Thanks and regards

0 项奖励
回复
14 回复数

906 次查看
Lubeiro
Contributor I

Hello

I know what DS says but I am not asking for static values but dynamic ones. It is not the same.

What about if there is -0.31V during 1ps? Will i.MX8 break?

Regards

0 项奖励
回复

1,178 次查看
joanxie
NXP TechSupport
NXP TechSupport

which imx8 processor do you use? imx8qm?

0 项奖励
回复

1,173 次查看
Lubeiro
Contributor I
i.MX8M Mini
0 项奖励
回复

1,100 次查看
joanxie
NXP TechSupport
NXP TechSupport

I checked the data sheet, nxp doesn't offer the overshoot and undershoot as percentage like TI, refer to the data sheet,  the minimum allowed undershoot is -0.3V and the maximum allowed overshoot is VDD+0.3V, this is 3.3v+0.3V=3.6v for 3.3v level signal

0 项奖励
回复

1,053 次查看
Lubeiro
Contributor I

My reply is being deleted, why?

0 项奖励
回复

1,031 次查看
joanxie
NXP TechSupport
NXP TechSupport

not receive any reply, you can post again

0 项奖励
回复

907 次查看
Lubeiro
Contributor I

Hello,

-0.31V during 1ps will damage i.MX8?

Regards

0 项奖励
回复

908 次查看
Lubeiro
Contributor I

Hello, Yes, I know what DS says but I'm not asking for static values but dynamic ones. It is not the same. What about if there is -0.31V for 1ps? will i.MX8 break? Regards

0 项奖励
回复

908 次查看
Lubeiro
Contributor I

Hello,

Yes, I know what DS says but I'm not asking for static values but dynamic ones. It is not the same.
What about if there is -0.31V for 1ps? will i.MX8 break?

Regards

0 项奖励
回复

906 次查看
Lubeiro
Contributor I

Hello,

Yes, I know what DS says but I'm not asking for static values but dynamic ones. It is not the same.
What about if there is -0.31V for 1ps? will i.MX8 break?

Regards

0 项奖励
回复

905 次查看
Lubeiro
Contributor I
Hello,

Yes, I know what DS says but I'm not asking for static values but dynamic ones. It is not the same.
What about if there is -0.31V for 1ps? will i.MX8 break?

Regards
0 项奖励
回复

905 次查看
Lubeiro
Contributor I
Hello joanxie,

I had already checked datasheet before i wrote this post. Statics values are only part of the information and they are not very useful since normally these values are exceeded specially in "fast strong" simulation (-40ºC , 1.95V).
What about if there is an undershoot of -0.31V during 1ps? Would i.MX8 be broken?

Regards
0 项奖励
回复

904 次查看
Lubeiro
Contributor I
Hello Joanxie,

I had already checked datasheet before i wrote this post. Statics values are only part of the information and they are not very useful since normally these values are exceeded specially in "fast strong" simulation (-40ºC , 1.95V).
What about if there is an undershoot of -0.31V during 1ps? Would i.MX8 be broken?

Regards
0 项奖励
回复

904 次查看
Lubeiro
Contributor I
Hello Joanxie,

I had already checked datasheet before i wrote this post. Statics values are only part of the information and they are not very useful since normally these values are exceeded specially in "fast strong" simulation (-40ºC , 1.95V).
What about if there is an undershoot of -0.31V during 1ps? Would i.MX8 be broken?
0 项奖励
回复