i.MX8 h.264 encoder bit rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8 h.264 encoder bit rate

ソリューションへジャンプ
1,292件の閲覧回数
ko-hey
Senior Contributor II

Hi all,
 
I have a question about H.264 encoder in i.MX8.
 
According to the reference manual(Table 15-8) of i.MX8MMini, the bit rate is as below.
Minimum: 10kbps
Maximum: 40 Mbps at 1080p 60 fps
 
How about is it in i.MX8 ?
 
Ko-hey

0 件の賞賛
返信
1 解決策
1,190件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

i.MX8 QM B0 supports two HW encoders each one associated to a Cortex-M0. Each HW encoder is capable of encoding 1x H.264 1080p30 or 2x H.264 720p30.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,190件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the imx8qm data sheet, for encoder, imx8QM supports up to 1080p@30,should be the 20M bps, no data for min

0 件の賞賛
返信
1,190件の閲覧回数
ko-hey
Senior Contributor II

Hi joanxie

It's worse than i.MX8MMini. Are you sure ?

Ko-hey

0 件の賞賛
返信
1,191件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

i.MX8 QM B0 supports two HW encoders each one associated to a Cortex-M0. Each HW encoder is capable of encoding 1x H.264 1080p30 or 2x H.264 720p30.

0 件の賞賛
返信