i.MX8 : facing issue while fetching latest source with repo sync

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8 : facing issue while fetching latest source with repo sync

797件の閲覧回数
vsuneja63
Contributor III

vipulkumar@A812DBLR:~/platform/AGL_Lamprey$ repo init -b lamprey -u https://gerrit.automotivelinux.org/gerrit/AGL/AGL-repo

Your identity is: vipul <vsuneja63@gmail.com>
If you want to change this, please re-run 'repo init' with --config-name

repo has been initialized in /home/vipulkumar/platform/AGL_Lamprey


vipulkumar@A812DBLR:~/platform/AGL_Lamprey$ repo sync
Fetching: 100% (30/30), done in 16.543s
Garbage collecting: 100% (30/30), done in 0.089s
info: A new version of repo is available
warning: repo is not tracking a remote branch, so it will not receive updates
repo reset: error: Entry 'SUBMITTING_PATCHES.md' not uptodate. Cannot merge.
fatal: Could not reset index file to revision 'v2.21^0'.

ラベル(1)
0 件の賞賛
返信
1 返信

762件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Note: Currently, we don't support for AGL.We will not provide any support if you have issue when using AGL.

0 件の賞賛
返信