i.MX8: creare buildroot linux for SOM-Q7-MX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8: creare buildroot linux for SOM-Q7-MX8

291 Views
Dali
Contributor I

Hi,

 

I would like to create a linux distribution via buildroot and use an sd card to boot the board SOM Q7 from seco.

 

The challenge is that I do not know which xconfig should I use?

 

Best regards

Mohamed-Ali Fahmy

0 Kudos
Reply
1 Reply

246 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Currently buildroot linux distributions are not maintained by NXP, I guess I could refer you to the buildroot documentation.

But I'd rather encourage you to create a linux distribution for your SOM with yocto as you could base on our BSP releases and port your board.

Regards

0 Kudos
Reply