i.MX8 booting from QSPIFlash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 booting from QSPIFlash

Jump to solution
4,496 Views
efio
Contributor III

Hi we've a imx8mn based board with different DDR chip and different NOR flash connected to QSPI interface. (different from imx8mn-evk board)
As well we have two boot options: eMMC and QSPI.
The board boots and works while booting from eMMC, the QSPI flash is available in u-boot and Linux.
But, when we're trying to switch to QSPI boot option - boot fails - no output on the console.
On the other hand, we can see the clocks on SPI bus and - it means the CPU indeed tries to boot from QSPI.
We're building our QSPI flash image with a help of imx-mkimage utility, there is a guide of how to create it:
https://community.nxp.com/t5/i-MX-Processors/IMX8Mnano-EVK-How-to-make-QSPI-booting-image/td-p/17047...
In addition, here is the out of: make SOC=iMX8MN DEV=flexspi flash_evk

BL32=tee.bin DEK_BLOB_LOAD_ADDR=0x40400000 TEE_LOAD_ADDR=0x56000000 ATF_LOAD_ADDR=0x00960000 ../iMX8M/mkimage_fit_atf.sh evk.dtb  > u-boot.its
bl31.bin size: 
41456
u-boot-nodtb.bin size: 
736416
evk.dtb size: 
28304
./mkimage_uboot -E -p 0x5000 -f u-boot.its u-boot.itb
FIT description: Configuration to load ATF before U-Boot
Created:         Tue Oct  8 17:44:52 2024
 Image 0 (uboot-1)
  Description:  U-Boot (64-bit)
  Created:      Tue Oct  8 17:44:52 2024
  Type:         Standalone Program
  Compression:  uncompressed
  Data Size:    736416 Bytes = 719.16 KiB = 0.70 MiB
  Architecture: AArch64
  Load Address: 0x40200000
  Entry Point:  unavailable
 Image 1 (fdt-1)
  Description:  evk
  Created:      Tue Oct  8 17:44:52 2024
  Type:         Flat Device Tree
  Compression:  uncompressed
  Data Size:    28304 Bytes = 27.64 KiB = 0.03 MiB
  Architecture: Unknown Architecture
 Image 2 (atf-1)
  Description:  ARM Trusted Firmware
  Created:      Tue Oct  8 17:44:52 2024
  Type:         Firmware
  Compression:  uncompressed
  Data Size:    41456 Bytes = 40.48 KiB = 0.04 MiB
  Architecture: AArch64
  OS:           Unknown OS
  Load Address: 0x00960000
 Default Configuration: 'config-1'
 Configuration 0 (config-1)
  Description:  evk
  Kernel:       unavailable
  Firmware:     uboot-1
  FDT:          fdt-1
  Loadables:    atf-1
41420+1 records in
41421+0 records out
165684 bytes (166 kB, 162 KiB) copied, 0.0578868 s, 2.9 MB/s
./mkimage_imx8 -version v2 -fit -loader u-boot-spl-ddr.bin 0x912000 -second_loader u-boot.itb 0x40200000 0x60000 -out flash.bin
Platform: i.MX8M (mScale)
ROM VERSION: v2
Using FIT image
LOADER IMAGE: u-boot-spl-ddr.bin start addr: 0x00912000
SECOND LOADER IMAGE: u-boot.itb start addr: 0x40200000 offset: 0x00060000
Output: flash.bin
fit_size: 886
1+0 records in
1+0 records out
886 bytes copied, 5.7108e-05 s, 15.5 MB/s
FIT hash: 9dc0d453c9a49e3d880292c4c330e685ea495c6856ab82ab61354b134f9b
========= IVT HEADER [HDMI FW] =========
header.tag: 0x0
header.length: 0x0
header.version: 0x0
entry: 0x0
reserved1: 0x0
dcd_ptr: 0x0
boot_data_ptr: 0x0
self: 0x0
csf: 0x0
reserved2: 0x0
boot_data.start: 0x0
boot_data.size: 0x0
boot_data.plugin: 0x0
========= IVT HEADER [PLUGIN] =========
header.tag: 0x0
header.length: 0x0
header.version: 0x0
entry: 0x0
reserved1: 0x0
dcd_ptr: 0x0
boot_data_ptr: 0x0
self: 0x0
csf: 0x0
reserved2: 0x0
boot_data.start: 0x0
boot_data.size: 0x0
boot_data.plugin: 0x0
========= IVT HEADER [LOADER IMAGE] =========
header.tag: 0xd1
header.length: 0x2000
header.version: 0x41
entry: 0x912000
reserved1: 0x0
dcd_ptr: 0x0
boot_data_ptr: 0x911fe0
self: 0x911fc0
csf: 0x9527c0
reserved2: 0x0
boot_data.start: 0x911fc0
boot_data.size: 0x42860
boot_data.plugin: 0x0
========= OFFSET dump =========
Loader IMAGE:
 header_image_off 0x0
 dcd_off 0x0
 image_off 0x40
 csf_off 0x40800
 spl hab block: 0x911fc0 0x0 0x40800
 
Second Loader IMAGE:
 sld_header_off 0x58000
 sld_csf_off 0x59020
 sld hab block: 0x401fadc0 0x58000 0x1020
 fit-fdt csf_off 0x5b020
 fit-fdt hab block: 0x401fadc0 0x58000 0x3020
SPL CSF block:
Blocks = 0x911fc0 0x0 0x40800 "flash.bin"
SLD CSF block:
Blocks = 0x401fadc0 0x58000 0x1020 "flash.bin",\
SLD FIT-FDT CSF block:
Blocks = 0x401fadc0 0x58000 0x3020 "flash.bin"
 
 

bootmode selected: FlexSPI - 3B Read '0110'

We can see on power up clock signal of the QSPI bus.
But we can't see the processor running. Nothing over the console.

  1.  What is probably incorrect in our FLASH image preparation?
  2. To which offset on QSPI FLASH the image should be burn?
  3. Do we need to config something on u-boot? SPL? if so, what to config?
The flash P/N we are using is: S25FL256SAGBHVB00

Thank you so much for your help,




Labels (1)
0 Kudos
Reply
1 Solution
3,910 Views
efio
Contributor III

Thank you for your previous assistance. I would like to provide a status update regarding the flash issue.

I've made progress by modifying the mkimage command to:

make SOC=iMX8MN DEV=flexspi flash_evk_flexspi

This resolved the initial problem as this command properly includes the QSPI header with the 0xFCFB word at address 0x400.

However, I'm now encountering a new issue when attempting to access the flash from U-Boot. Specifically, the "sf probe" command fails with the following error:

u-boot=> sf probe

Invalid bus 0 (err=-19)

Failed to initialize SPI flash at 0:0 (error -19)

Notably, when booting from eMMC and stopping at U-Boot, the "sf probe" command works correctly. This suggests that the controller might be holding the bus, preventing access to the flash.

Could you please provide guidance on how to properly configure or release the bus controller in this scenario?

Thank you for your continued support.

 

Best regards

View solution in original post

0 Kudos
Reply
22 Replies
3,627 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @efio 

Glad to here that. You are welcome. And for the further question, Could you please create another ticket talk about it?

B.R

0 Kudos
Reply
3,911 Views
efio
Contributor III

Thank you for your previous assistance. I would like to provide a status update regarding the flash issue.

I've made progress by modifying the mkimage command to:

make SOC=iMX8MN DEV=flexspi flash_evk_flexspi

This resolved the initial problem as this command properly includes the QSPI header with the 0xFCFB word at address 0x400.

However, I'm now encountering a new issue when attempting to access the flash from U-Boot. Specifically, the "sf probe" command fails with the following error:

u-boot=> sf probe

Invalid bus 0 (err=-19)

Failed to initialize SPI flash at 0:0 (error -19)

Notably, when booting from eMMC and stopping at U-Boot, the "sf probe" command works correctly. This suggests that the controller might be holding the bus, preventing access to the flash.

Could you please provide guidance on how to properly configure or release the bus controller in this scenario?

Thank you for your continued support.

 

Best regards

0 Kudos
Reply
3,655 Views
efio
Contributor III

Hi,

I am pleased to inform you that the issue has been fully resolved. The root cause was identified as an incorrect mkimage file configuration.

Thank you for your valuable assistance throughout this process.

Best regards,

0 Kudos
Reply
3,783 Views
pengyong_zhang
NXP Employee
NXP Employee

HI @efio 

Please use the following command compile your flash.bin file.

make SOC=iMX8MN flash_evk_flexspi

B.R

0 Kudos
Reply
3,885 Views
pengyong_zhang
NXP Employee
NXP Employee

HI @efio 

I found the same issue with you, You can refer it follow the below link. hope it can help you.

https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-QSPI-booting-and-partition/m-p/1661476

B.R

0 Kudos
Reply
3,801 Views
efio
Contributor III

Hi,

Unfortunately, the link doesn't help - I want to boot the imx8mn from the QSPI flash - meaning u-boot should come-up from the QSPI flash.

Any other suggestions? 


Thank you very much,

0 Kudos
Reply
3,938 Views
pengyong_zhang
NXP Employee
NXP Employee

hi @efio 

What is your result when you use the UUU command flash your .bin file?

B.R

0 Kudos
Reply
3,918 Views
efio
Contributor III
Same, doesn't work
0 Kudos
Reply
4,003 Views
pengyong_zhang
NXP Employee
NXP Employee

hi @efio 

I have some confuse about your schematic, you connect on flash, why your schematic have two flash chips?  My understand is you only connect S25FL256SAGBHVB00 , right?

And what is your command to flash your .bin file to your flash?

B.R

0 Kudos
Reply
3,989 Views
efio
Contributor III

Hi,

It's only one flash, the symbol package is divided to two for convenience.
I flashed the data using external J-Link and using dd command of linux.
both gave some results.

Hexdump gives the correct data.

I don't think the data is the issue, something is wrong what the IVT header the QSPI controller reads.

========= IVT HEADER [LOADER IMAGE] =========
header.tag:             0xd1
header.length:          0x2000
header.version:         0x41

Thank you,

0 Kudos
Reply
4,061 Views
pengyong_zhang
NXP Employee
NXP Employee

HI @efio 

Could you please share your board schematic file and your nor flash datasheet file?

B.R

0 Kudos
Reply
4,051 Views
efio
Contributor III

Hi,

Yes of course, you can see below the schematics for both QSPI Flash and imx8mn.
Please note that I can see the signals over scope and I can communicate with the flash in uboot & linux (read, write and more). The issue occurs only when trying to boot from the QSPI flash.
The mux in the schematics meant for external flash burning - which also works.

As I wrote before about observations of the QSPI controller:

  1. Using an oscilloscope, I monitored the SPI wave and noticed the QSPI controller reading address 0x400 with command 0x3.
  2. The read register value is 0xd1002041, which I believe should be correct.
  3. The controller attempts this read twice.
  4. A third read attempt is made using command 0x13 (4-byte address read), resulting in the same value: 0xd1002041.
  5. After these three cycles, the operation halts.

Any suggestions?

Thank you,

 

QSPI Flash sideQSPI Flash sideimx8mn sideimx8mn side

0 Kudos
Reply
4,045 Views
efio
Contributor III

Flash data sheet:
S25FL256SAGBHVB00 

0 Kudos
Reply
4,141 Views
pengyong_zhang
NXP Employee
NXP Employee

hi @efio 

you are use our NXP i.MX8MN evk board or customer's board?

 

0 Kudos
Reply
4,102 Views
efio
Contributor III

Hi,

Customized board,

0 Kudos
Reply
4,156 Views
efio
Contributor III

Does the entry: 0x912000 correct for imx8mn?

0 Kudos
Reply
4,176 Views
pengyong_zhang
NXP Employee
NXP Employee

hi @efio 

I have test this on  my i.mx8mn evk board. And no issue found. Please share your uuu command result.

"uuu -b qspi <.bin file>"

B.R

0 Kudos
Reply
4,165 Views
efio
Contributor III

Hi,

Using uuu didn't work. I see that the flash is burned using sf read.
Is there any offset I should burn the bin file or it supposed to be in address 0x0?

Thank you

0 Kudos
Reply
4,200 Views
pengyong_zhang
NXP Employee
NXP Employee

HI @efio 

Did you choose the right boot selection? Please refer the following Boot selection for i.mx8MN.

pengyong_zhang_0-1728549935338.png

B.R

 

0 Kudos
Reply
4,198 Views
efio
Contributor III

Hi,

 

Yes I did,

0 Kudos
Reply