Hi Sir,
I have a problem about GPIO setting on i.MX8 EVK. The problem is all GPIO pins do not have high/low change after I exported them.
For example:
echo 489 > /sys/class/gpio/export
echo out > /sys/class/gpio/gpio489/direction
echo 1 > /sys/class/gpio/gpio489/value
root@imx8qxpmek:~# cat /sys/kernel/debug/gpio
......
gpiochip0: GPIOs 480-511, parent: platform/5d080000.gpio, 5d080000.gpio:
gpio-489 ( |sysfs ) out hi
echo 0 > /sys/class/gpio/gpio489/value
root@imx8qxpmek:~# cat /sys/kernel/debug/gpio
......
gpiochip0: GPIOs 480-511, parent: platform/5d080000.gpio, 5d080000.gpio:
gpio-489 ( |sysfs ) out lo
The scope does not measure high/low output change after above steps. Have anyone know why? Below is my pinmux setting in dts file.
pinctrl_testb: testgrp{
fsl,pins = <
SC_P_ESAI0_FST_LSIO_GPIO0_IO01 0xE0000021 // IMX_GNSS_TXREADY (in)
SC_P_ESAI0_SCKR_LSIO_GPIO0_IO02 0xE0000021 // VBAT_FAIL_N (in)
SC_P_ESAI0_SCKT_LSIO_GPIO0_IO03 0xE0000021 // M_SLEEP (in)
SC_P_ESAI0_TX0_LSIO_GPIO0_IO04 0xE0000021 // BT_EN (out)
SC_P_ESAI0_TX1_LSIO_GPIO0_IO05 0xE0000021 // WLAN_EN (out)
SC_P_ESAI0_TX2_RX3_LSIO_GPIO0_IO06 0xE0000021 // M_SHUTDOWN (out)
SC_P_ESAI0_TX3_RX2_LSIO_GPIO0_IO07 0xE0000021 // WLAN_SLP_CLK (out)
SC_P_ESAI0_TX4_RX1_LSIO_GPIO0_IO08 0xE0000021 // USB_HUB_RST_N (out)
SC_P_ESAI0_TX5_RX0_LSIO_GPIO0_IO09 0xE0000021 // M_RUN (out)
SC_P_SPDIF0_RX_LSIO_GPIO0_IO10 0xE0000021 // MODE1 (in)
SC_P_SPDIF0_TX_LSIO_GPIO0_IO11 0xE0000021 // MODE2 (in)
SC_P_SPDIF0_EXT_CLK_LSIO_GPIO0_IO12 0xE0000021 // IMX_GNSS_RESET (out)
>;
};
pinctrl_gpio1: gpio1grp{
fsl,pins = <
SC_P_ADC_IN5_LSIO_GPIO1_IO13 0xE0000021 // HDMI_INT (in)
SC_P_ADC_IN4_LSIO_GPIO1_IO14 0xE0000021 // M_WAKEUP_1V8 (in)
>;
};
pinctrl_gpio4: gpio4grp{
fsl,pins = <
SC_P_USDHC1_VSELECT_LSIO_GPIO4_IO20 0xE0000021 // SD1_VSELECT (out)
SC_P_USDHC1_WP_LSIO_GPIO4_IO21 0xE0000021 // GNSS_1PPS (in)
>;
};
.....
&gpio0 {
pinctrl-name = "default";
pinctrl-0 = <&pinctrl_testb>;
// pinctrl-0 = <&pinctrl_gpio0>;
status = "okay";
};
&gpio1 {
pinctrl-name = "default";
pinctrl-0 = <&pinctrl_gpio1>;
status = "okay";
};
&gpio4{
pinctrl-name = "default";
pinctrl-0 = <&pinctrl_gpio4>;
status = "okay";
};
// End of added by Kevin 20181008 -- for H7.1E GPIO group
&gpio5 {
pinctrl-names = "default";
// pinctrl-0 = <&pinctrl_testb>;
pinctrl-0 = <&pinctrl_gpio5>;
status = "okay";
};
Best regards
Kevin
Hi Kevin
what board and processor used in the case. If it is i.MX8M EVK
then used bsp is wrong based on log: "root@imx8qxpmek" -
this is for i.MX8QXP MEK board which is different from i.MX8M EVK.
i.MX8QXP is not publicly released yet and not officially supported.
For i.MX8M EVK one can use Linux 4.9.88
Documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------