In the i.MX8 Mini EVK which just bought without doing anything, and using your OS which had already burn in the NAND FLASH.
I have seen the BT icon in the system,but why the BT function cannot be use?
Thanks
did you use nxp imx8mm ddr4 board? which bsp version do you use?
Yes, I use imx8mm DDR4 EVK, and it show "Unavailable" on BT address.
Andriod 9
Kernel version :4.14.98-00063-gbcdaf61 #1 Sun Apr 7 02:27:35 CST 2019
could you send me the picture of "Unavailable" ? I flashed the P9.0.0_2.0.0 images to the IMX8MM DDR evk SD card, doesn't have the same issue as yours, refer to the schematic and user guide, The BCM 1MW Wi-Fi/Bluetooth module is used on the i.MX 8M Mini EVK DDR4 Board.
Besides, I tried to use command "rfkill" to open BT through debug port.
But It shows nos such command.
Is there any solution ?
Thanks.
what android 9 do you need to use? I need to download the source code to check if current bsp enable it or not