i.MX8 MIPI rate question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 MIPI rate question

1,772 Views
xu_ji1
Contributor V

Hello,

We used i.MX8QP and Ti DS960 deserializer as transform camera data.

When set ds960 CSI TX data rate to 1.2Gbps,connect four 1080P cameras capture image at same time,

all images are no problem;when set ds960 CSI TX data rate to 1.6Gbps,

connect four 1080P cameras capture image at same time,

all images data not good,some pixel data missing.

 

What makes this problem?does i.MX8 not support high MIPI data rate?

Tags (1)
0 Kudos
12 Replies

1,660 Views
xu_ji1
Contributor V

hello,

 

How about the conclution? Do i.MX8QP and i.MX8QXP support 4X1080P@30fps cameras at 1.6Gbps TX?

0 Kudos

1,658 Views
joanxie
NXP TechSupport
NXP TechSupport

I only can say for imx8qm or imx8qxp side, which can support 4x1080p@30 with 16bpp, if you need to support this, you need enable 4-lane, For 1080P30 camera, its pixel clock is about 74.25Mhz, so for each if use 16bpp data rate = 74.25M * 16bpp = 1188Mbps. So 4xcamera bandwidth is 4.752Gbps.

 

0 Kudos

1,635 Views
xu_ji1
Contributor V

Where is enabled the 4-lanes on i.MX8QP?pls give detail guide

0 Kudos

1,621 Views
joanxie
NXP TechSupport
NXP TechSupport

data-lanes = <1 2 3 4>; this is for data lane settings,since you set the four 1080p camera successfully when you set the DS960 to 1.2G, but failed when you set DS960 to 1.6G, which means that imx8qm can support 4 1080p camera, you should check the DS960 settings

0 Kudos

1,753 Views
joanxie
NXP TechSupport
NXP TechSupport

what's camera settings different from DS960  1.2G to 1.6G? you can calculate by yourself, the imx8qp supports up to 6Gbps, if your 4 camera is 1080p 16bpp, should be 148.5Mx16bppx4>6Gbps

 

 

0 Kudos

1,749 Views
xu_ji1
Contributor V

camera setting not diff with 1.2G and 1.6G,only ds960 CSI TX rate register setting diff.

why 1.2G setting is ok for i.mx8qp?

How about 148.5M? how to calculate it?

0 Kudos

1,767 Views
joanxie
NXP TechSupport
NXP TechSupport

for imx8qp, The MIPI CSI-2 IP provides MIPI CSI-2 standard camera interface ports. The MIPI
CSI-2 interface supports up to 1.5 Gbps for up to 4 data lanes

when you use the 1.6Gbps, did you set the imx8qp mipi csi as 4 lanes?

 

0 Kudos

1,742 Views
joanxie
NXP TechSupport
NXP TechSupport

do you use DS90UB960? as I known DS90UB960 supportts 4lane, maybe you need to check the DS90UB960 side, I think maybe your DS90UB960 set as 1.6Gx4lane?? since 1.2G can support 4 1080p camera, why do you need to change to 1.6G? we don't test DS90UB960 ever, but tested MAX9286 with 4 camera successfully

 

0 Kudos

1,741 Views
xu_ji1
Contributor V

yes it is DS90UB960,I just want to check the max mipi rate of platform,

previous said the imx8qp supports up to 6Gbps,and 1.6G with 4X1080P cameras >6Gbps,

is it keypoint?

MAX9286 support 4X1280X800 cameras as I know.

and also I try it on i.MX8QXP ds960 set 1.2G can not support 4X1080P cameras,only support 3X1080P+

1X720P cameras,what is 8QXP supports up?

0 Kudos

1,704 Views
joanxie
NXP TechSupport
NXP TechSupport

what frame rate do you use for all of your user case??

 

0 Kudos

1,701 Views
xu_ji1
Contributor V

30fps

0 Kudos

1,766 Views
xu_ji1
Contributor V

Hello,

Where set mipi csi as 4lanes, in my dtsi has code:

&mipi_csi_0 {
#address-cells = <1>;
#size-cells = <0>;
virtual-channel;
status = "okay";

/* Camera 0 MIPI CSI-2 (CSIS0) */
port@0 {
reg = <0>;
mipi_csi0_ep: endpoint {
remote-endpoint = <&ds960_0_ep>;
data-lanes = <1 2 3 4>;
};
};
};

 

is it ok?

0 Kudos