Hi,
I am using i.MX8QXP custom board with 4.9.88_beta 2 SDK to develop.
We connect 2 spi slave devices to the LPSPI3 port, but I found the SPI3_CS1 can not config to GPIO.
In the spi-fsl-lpspi.c , the chipselect should be gpio to let the driver control which spi device to be select.
So my questions are
1. In LPSPI3 , the driver how to control SPI3_CS1 if this pin can not config to GPIO
2. IF SPI3_CS0 , SPI3_CS1 can be set to gpio , what is the correct representation in dts ?
like below ??
cs-gpios = <&gpio1 16 GPIO_ACTIVE_LOW> , <&gpio1 17 GPIO_ACTIVE_LOW> ,
spi-fsl-lpspi.c
for (i = 0; i < master->num_chipselect; i++) {
int cs_gpio = of_get_named_gpio(np, "cs-gpios", i);if (!gpio_is_valid(cs_gpio) && lpspi_platform_info)
cs_gpio = lpspi_platform_info->chipselect[i];fsl_lpspi->chipselect[i] = cs_gpio;
if (!gpio_is_valid(cs_gpio))
continue;ret = devm_gpio_request(&pdev->dev, fsl_lpspi->chipselect[i],
DRIVER_NAME);
if (ret) {
dev_err(&pdev->dev, "can't get cs gpios\n");
goto out_master_put;
}
}
my spi3 dts part
pinctrl_lpspi3: lpspi3grp {
fsl,pins = <
SC_P_SPI3_SCK_ADMA_SPI3_SCK 0x0600004c
SC_P_SPI3_SDO_ADMA_SPI3_SDO 0x0600004c
SC_P_SPI3_SDI_ADMA_SPI3_SDI 0x0600004c
SC_P_SPI3_CS1_ADMA_SPI3_CS1 0x0600004c
>;
};pinctrl_lpspi3_cs0: lpspi3_cs0 {
fsl,pins = <
SC_P_SPI3_CS0_LSIO_GPIO0_IO16 0x21>;
}&lpspi3 {
#address-cells = <1>;
#size-cells = <0>;
fsl,spi-num-chipselects = <2>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lpspi3 &pinctrl_lpspi3_cs0>;
cs-gpios = <&gpio1 16 GPIO_ACTIVE_LOW>;
status = "okay";
spidev@0 {
compatible = "rohm,dh2228fv";
spi-max-frequency = <500000>;
reg = <0>;
}spidev@1 {
compatible = "rohm,dh2228fv";
spi-max-frequency = <500000>;
reg = <0>;
};
};
Best,
Andy
Hi Andy and Sharmila,
How did you work around this issue? I got into the same issue.
Thanks,
Dionie
You have two chipselects but only configure 1 gpio in cs-gpios.
For your examples, you may refer to this:
Hi Jimmy,
Thanks for your reply.
But as I said, in the i.MX8 platform, I can not config the SPI3 CS1 to GPIO.
There is no GPIO option for SPI3 CS1 .
Do you have any comment ?
Best,
Andy
Hi Jimmy,
I am also working on i.MX8 platform, we do use SPI3 and as you told we cannot configure SPI3 CS1 to GPIO. The lpspi driver doesnot support native chip select. So I have the issue with chip select. Problem is chip select is not going low. Do you have any suggestions/solution on this ?
Regards,
Sharmila