i.MX8 Boot failure in custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 Boot failure in custom board

991 Views
baraths
Contributor I

Dear Team,

The issue occurs in loading the kernel by uboot. (The same image with SD Card has been verified booting in EVK)
The following are some of the methods we tried to address this issue,
1. Suspected LPDDR4 issue:
    Testing performed using the below tool provided by NXP to confirm the DDR interface is as expected.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

    below link for ddr tool user guide document.

https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/138583/2/MSCALE_DDR_Tool_...
The DDR_Log.txt file contains the log of Stress test and calibration performed on DDR memory.

2. Suspected custom built image:
    Referred to the below link provided by NXP which contains default built images,

Procedure to flash the bootloader to sdcard using uuu tool

 sudo ./uuu -b sd ./imx-boot

below command is to flash the all images to sdcard using uuu tool

sudo ./uuu -b sd_all ./imx-boot ./ubuntu-rootfs-imx8mm.wic

With the above image only Partial kernel was booted and the processor hangs. Attached "SDcard_boot_log.txt" for reference.

 

Regards,

Barath.S

Labels (1)
0 Kudos
Reply
0 Replies