i.MX7ULP SAI Channels Using

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX7ULP SAI Channels Using

540 次查看
ATAineri
Contributor III

Good afternoon, dear NXP! I Can't understand from datasheet:

For example, SAI0 has 2 RX and 2 TX channels. I'm going to develop dual mono Digital Audio Player. It means that there is 2 DAC microchips: 1 for L and 1 for R.

I can't understand from Linux Kernel Module - is this 2 channels is L and R reletivetely or it is something another and I have to use TX0 for both channels and SYNC lane is signalize - what channel DAC have to read?

Now - I can't understand how to realize dual mono DAP using i.MX7ULP SAI

Is there some drivers that I can read to understand how it works or I should write my own driver to provide such functionality?

标签 (5)
0 项奖励
1 回复

529 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vladislav

 

> is this 2 channels is L and R reletivetely or it is something another and I

>have to use TX0 for both channels and SYNC lane is signalize - what channel DAC have to read?

 

2 channels are not for L and R , one TX0 can be used for L and R, for usage one can look

at wm8960 example in i.MX7ULP EVK schematic (p.9 SPF-29164)   MCIMX7ULP-EVK Design Files

Driver description can be found in  i.MX Linux Reference Manual​

 

Best regards
igor

0 项奖励