i.MX7ULP: IO configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7ULP: IO configuration

828 Views
mrudangshelat1
Senior Contributor II

Hi,

I am planning to use imx7ULP in one of the medical applications device. And require 3 Mic to interface with iMX7ULP. And it is battery operated device so we have to select iMX7ULP. I have some of the query below kindly provide suitable answers.

  1. Are Flex IO can be configured for I2S or not?
  2. What is the minimum m4 operating frequency?

Mrudang

Labels (1)
8 Replies

668 Views
mrudangshelat1
Senior Contributor II

Hi Igor,

Can you provide me the steps to go below 48MHz for M4 core?

Mrudang

0 Kudos

668 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

please refer to sect.26.1.4 Instantiation information for SCG0 (M4)

i.MX 7ULP Applications Processor Reference Manual

Best regards
igor

668 Views
mrudangshelat1
Senior Contributor II

Hi Igor,

Thanks for your support and quick response.

Mrudang

0 Kudos

668 Views
mrudangshelat1
Senior Contributor II

Hi Igor,

Just confirm that by using the below application note. we can convert any FLEXIO of M4 and A7 to SAI, I2C etc...

https://www.nxp.com/docs/en/application-note/AN4955.pdf 

https://www.nxp.com/docs/en/application-note/AN12174.pdf 

Please confirm

Mrudang

0 Kudos

668 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

yes these app notes can be used as starting point.

Best regards
igor

668 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

>Are Flex IO can be configured for I2S or not?

yes, one can refer to below app notes:

https://www.nxp.com/docs/en/application-note/AN4955.pdf 

https://www.nxp.com/docs/en/application-note/AN12174.pdf 

>What is the minimum m4 operating frequency?

no limit for minimum frequency.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

668 Views
mrudangshelat1
Senior Contributor II

Hi Igor,

I will take a look. 

I have seen the min freq is 48MHz in Very Low Power Run (VLPR) for M4. Can we go below that?

Mrudang

0 Kudos

668 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

>I have seen the min freq is 48MHz in Very Low Power Run (VLPR) for M4. Can we go below that?

yes

Best regards
igor

0 Kudos