i.MX7ULP_EVB USB OTG enable problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7ULP_EVB USB OTG enable problem

1,596件の閲覧回数
sam_liu
Contributor II

Hi Everyone,

  I have some questions about how should I do that can correctly enable USB OTG on i.MX7ULP_EVB. 

  (BSP version : imx-4.9.51-8mq_ga.).

  My purpose is :

  Setting i.mx7ulp_evb as a "USB device" , and connect the Type-C USB port(It's is locate on i.mx7ulp_evb )  into my PC , let my PC can recognize i.mx7ulp_EVB as a USB device (eg. A mass storage)

 

But now my PC can't recognize  the i.mx7ulp_evb as a USB device.

  And I already according to "i.MX Reference Manual ,Document Number: IMXLXRM ,Rev. L4.9.51_imx8mq-beta, 01/2018" to setting parameters (These parameters almost default :y in BSP) :

 ============================================================

1. CONFIG_USB-Build Support for Host-side USB
2. CONFIG_USB_EHCI_HCD EHCI HCD (USB 2.0) support
Default y
3. CONFIG_USB_CHIPIDEA- ChipIdea high-speed Dual Role Controller
Default y
4. CONFIG_USB_CHIPIDEA_UDC - ChipIdea device controller
Default y
5. CONFIG_USB_CHIPIDEA_HOST - ChipIdea host controller
Default y
6. CONFIG_USB_GADGET - USB Gadget Support
Default y
7. CONFIG_USB_MXS_PHY - Freescale MXS USB PHY support
Default y

=============================================================

My question show as below:

1. The parameter : "OTG support " in menuconfig:

    ---Device drivers 

       ---USB support 

           [ ] OTG support  <-------   Does this parameter should set to "y" ?

2.In the original  "i.mx7ulp_evk.dts" in "imx-4.9.51-8mq_ga BSP" , the  CC Logic Control : PTN5150A(it's for type-c driver ) is not setting .

   Should I need to add device node PTN5150A  manually or not?

3.Why I can't find  the 

"/sys/bus/usb/devices/usb1"

and 

"/sys/bus/usb/devices/1-1"  in i.mx7ulp linux kernel environment.

4.In original "&usbotg1" node in "i.mx7ulp_evk.dts" as below :

------------------------------------------------------

&usbotg1 {
vbus-supply = <&reg_usb_otg1_vbus>;
extcon = <0>, <&extcon_usb1>;
srp-disable;
hnp-disable;
adp-disable;
status = "okay";
}; 

----------------------------------------------------

It's neither set 

dr_mode = "host"

nor 

dr_mode ="peripheral"

nor

dr_mode = "otg" 

    Should I need to add "dr_mode = "otg"   into or not?

5.In the menuconfig ,whether any parameters of my setting is incorrect?

6.What steps should I do that  can enable USB otg correctly?

Thanks.   

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,055件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  Note, i.MX 7ULP is not launched and supported yet.

Nevertheless, in general, some questions may be answered as following:

 

1.

  Yes, OTG support is needed.

 

2.

  USB type-C and PD stack is supported for i.MX8.

Customers can try to implement own solution for i.MX 7ULP.

 

3.

  You may try the recent NXP Linux BSP L4.9.88.

 

4.

  At least You may try to add "dr_mode = "otg".


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信