Hello
I'm using U-Boot based on v2018.11 + CONFIG_SECURE_BOOT.
The M4 hello world (FreeRTOS) example is not functioning when the U-Boot is compiled with CONFIG_SECURE_BOOT.
An attempt was made to load the example to the following sections:
Thanks,
Uri
Hello,
is it possible to look at the log, demonstrating the issue?
Regards,
Yuri.
Hello Yuri,
No messages are generated.
Is there a way to check the status the M4 core?
Thanks,
Uri
Hello,
Can, at least, U-boot run?
Regards,
Yuri.
Hi Yuri,
It seems that the U-Boot is not affected:
U-Boot # tftp 7F8000 hello_world.bin
Using FEC0 device
TFTP from server 192.168.11.218; our IP address is 192.168.122.85
Filename 'hello_world.bin'.
Load address: 0x7f8000
U-Boot # dcache flush
U-Boot # bootaux 7F8000
U-Boot #
Thanks,
Uri
Hello,
I've sent You i.MX Boot Utility to analyze boot log. Hope it helps.
Regards,
Yuri.