i.MX7D peripheral pins different power groups?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX7D peripheral pins different power groups?

500 次查看
thomaskofoedhan
Contributor III

I'm trying to configure the pin muxing using the Pins tool, but I keep getting peripherals with pins from different power groups. This makes it very hard to control which banks should be which voltage. Even the keypad pins which I'm working on at the moment can not all come from the same power bank. Is this correct or is there an error in the tool?

标签 (1)
0 项奖励
回复
1 回复

416 次查看
Yuri
NXP Employee
NXP Employee

Hello

   This is correct - some signals for modules, say for keypad, may be powered via different
power domains.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 项奖励
回复