[i.MX7D][Yocto 2.1] How to test PCIe eye pattern

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[i.MX7D][Yocto 2.1] How to test PCIe eye pattern

513 Views
alex_cheng1
Contributor I

I want to test PCIe eye pattern for i.MX7 Dual core.
Can you tell me the method of PCIe eye pattern test?

Thank you.

Best Regards,
Alex Cheng

Labels (2)
0 Kudos
1 Reply

409 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alex

one can try to follow sect.2.1 TX test configuration and procedures

AN4784 PCIe Certification Guide

https://www.nxp.com/docs/en/application-note/AN4784.pdf 

according to footnote 2 on p.3 :

2. After a far-end termination is determined to be present, the Link Training and

Status State Machine (LTSSM) enters the polling.compliance state and begins transmitting

the compliance pattern on all lanes. Users do not need to enter
any command to force the system into the polling.compliance state after boot.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos