i.MX7D Sabre(MCIMX7SABRE) with E-INK panel(X-IMXEBOOKDC4) : Xserver & Touchscreen support available ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7D Sabre(MCIMX7SABRE) with E-INK panel(X-IMXEBOOKDC4) : Xserver & Touchscreen support available ?

3,668 Views
shrikant_bobade
Contributor III

Hi,

I am using i.MX7D Sabre(MCIMX7SABRE) with E-INK panel(X-IMXEBOOKDC4) to check the display, I have downloaded pre-build image: L4.1.15_2.0.0-ga_images_MX7DSABRESD.tar.gz with md5sum: 167fceda879c814280924b05c4e48317 located at download
used contents: fsl-image-validation-imx-x11-imx7d.sdcard; zImage; u-boot-imx7dsabresd_epdc.imx; zImage-imx7d-sdb-epdc.dtb

Using above setup I am able to get the EPDC display initialized well.
Even the validation with imx-lib as guided @ https://community.nxp.com/docs/DOC-328663 worked out of box.
Using mxc_epdc_v2_fb_test.out able to get the various unit tests executed well on display.

Moving further I would like to check E-INK panel(X-IMXEBOOKDC4) supported with Xserver and Touchscreen support?

1. Observed fsl-image-validation-imx-x11-imx7d.sdcard booting with OE banner then Xserver won't acquire the E-INK display. Also observed X11 imx-test for epdc was explicitly removed /unit_tests/mxc_epdc_x11_fb_test.out @ ref https://bugzilla.yoctoproject.org/show_bug.cgi?id=3615
apart from it I didn't found out particular X11 validation for epdc display,

is Xserver support available for E-INK panel(X-IMXEBOOKDC4) ?

2. Is E-INK panel(X-IMXEBOOKDC4) have touchscreen support?

3. any pointers on getting schematic/documents for E-INK panel(X-IMXEBOOKDC4)?

Please advise, sharing pointers or references if any will be a great help.

Thanks
Shrikant

4 Replies

2,485 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Shrikant,

For Touch issues please check:

EPD Touch and Booting problem 

https://community.nxp.com/message/919809 

There are no special x11 unit tests, in unit_test one can find test sources which can be used for custom testing or developing new drivers. xserver for MX7 run on xf86-config, please check your BSP recipes-graphics/xorg-xserver/.

Also check how to verify the EPDC functionality:

How to verify EPD panel functionality 

To get the X-IMXEBOOKDC4 schematic, under NDA you migth have to apply to your local FAE. 

Hope it helps

2,485 Views
shrikant_bobade
Contributor III

Thanks! @Bio_TICFSL  for providing the details, I am going through it & I will get back with further difficulties/queries if any.

Thanks

Shrikant

2,485 Views
shrikant_bobade
Contributor III

Hi Bio_TICFSL

Please have a look, I have tried with my BSP specific xf86-config

But didn't got xserver running.

For elan-touch: I am also facing similar error @ elan touch driver error 

Please advise!

Thanks

Shrikant

0 Kudos
Reply

2,485 Views
senthilkumarcha
Contributor III

Hi ShrikantBobade,
Did you test the Xserver in EPDC ? 

If Yes, can you post how you solved the issues ?

Thanks

C.Senthilkumar

0 Kudos
Reply