Hello!
I am about to select a NAND flash for a hardware design based on the i.MX7D.
What is throwing me off is the Flashs "ECC requirement" of either 1 or 4 bits.
Integrated Silicon Solution Inc. SRAM, DRAM, FLASH, ANALOG, KGD, WAFER
From what I read in the MX7 datasheet, BCH performs ECC calculations for NAND operations and supports 2...62 bit ECC. Does this limit my NAND selection to 4-bit ECC versions?
If the selection is not limited, would you recommend 1- or 4-bit ECC? Never worked with NAND before so I am wondering if there are any (dis)advantages to either solution.
已解决! 转到解答。
Hi Lars
selection is not limited as with 2bit ecc settings bch will also work fine with 1bit ecc nands.
There are no preferences using 1- or 4-bit ecc nands.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Lars
selection is not limited as with 2bit ecc settings bch will also work fine with 1bit ecc nands.
There are no preferences using 1- or 4-bit ecc nands.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------