i.MX7D NAND 4-bit vs 1-bit ECC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7D NAND 4-bit vs 1-bit ECC

ソリューションへジャンプ
2,472件の閲覧回数
demoniacmilk
Contributor IV

Hello!

I am about to select a NAND flash for a hardware design based on the i.MX7D.

What is throwing me off is the Flashs "ECC requirement" of either 1 or 4 bits.

Integrated Silicon Solution Inc. SRAM, DRAM, FLASH, ANALOG, KGD, WAFER 

From what I read in the MX7 datasheet, BCH performs ECC calculations for NAND operations and supports 2...62 bit ECC. Does this limit my NAND selection to 4-bit ECC versions?

If the selection is not limited, would you recommend 1- or 4-bit ECC? Never worked with NAND before so I am wondering if there are any (dis)advantages to either solution.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,839件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lars

selection is not limited as with 2bit ecc settings bch will also work fine with 1bit ecc nands.

There are no preferences using 1- or 4-bit ecc nands.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,840件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lars

selection is not limited as with 2bit ecc settings bch will also work fine with 1bit ecc nands.

There are no preferences using 1- or 4-bit ecc nands.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信