i.MX7D: How to boot a u-boot image from RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7D: How to boot a u-boot image from RAM

1,739件の閲覧回数
tom_foy
Contributor I

I'd like to test a u-boot image from RAM on the i.MX7D, before I program it to Non-Volatile storage

My procedure is as follows:

- Use "loadb" to transfer the file u-boot.imx:

   => loadb 0x80800000

- Use kermit to send the file (works successfully)

- Run the new u-boot.imx image:

=> go 0x80800000

But the new image fails to boot and nothing is displayed on the console. I have run this process many times in the past on i.MX6 processors, but never on the i.MX7D.

I'm using both the Rocko & Warrior Yocto releases from NXP. I have tried the u-boot.bin image instead of the u-boot.imx --> no success.

Any help appreciated.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,644件の閲覧回数
tom_foy
Contributor I

Thanks Weidong - that looks like the way to go on this.

Cheers!

Tom

0 件の賞賛
返信

1,643件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Tom,

    Now we released uuu tools for writing images to target board based on i.MX processors via USB OTG port. you can use uuu tool to do it.

   Attachment is version 1.3.136, in it, there is uuu.exe and uuu.pdf ( how to use). If you want to get other version, you can check uuu.pdf, and get links for download.

Have a nice day!

B.R,

Weidong

0 件の賞賛
返信