Hello gusarambula,
my problem is a bit different:
just renaming the Firmware epdc_ED060XH2C1.fw supplied with the Sabre board to epdc_ED133UT2.fw and making the above modification to the Kernel
static struct fb_videomode config2_mode = {
.name="ED133UT2",
......
everything works quite well
Only if I run the test
mxc_epdc_v2_fb_test.out -n 18
some characters of the text have less contrast than the nearby ones.
Instead if I work with the correct fw file for ES133UT2 given to me by the local NXP FAE I have the following problems:
-At the boot the edpc display is cleared but the splash image is not drawn
-the splash image is drawn the first time I run the epdc test program or my epdc program
-the clear function doesn't work:each new image is superimposed on the previous one
Hello gusarabula,
I'm back from holiday, but I still have the same problem.
I'm working with Sabre imx7D and the 13"eink display ED133UT2.
If in the file mxc_epdc_v2_fb.c I set the parameters of ED060XH2C display with the correct x,y resolution of ED133UT2 and I upload to /lib/firmware/imx/epdc the fw "epdc_ED060xh2c1.fw" just after renaming it "epdc_ES133UT2.fw" everything works quite well:
static struct fb_videomode es133ut2mode = {
.name = "ES133UT2",
.refresh = 75,
.xres = 1600,
.yres = 1200,
.pixclock = 80000000,
.left_margin = 12,
.right_margin = 76,
.upper_margin = 4,
.lower_margin = 5,
.hsync_len = 12,
.vsync_len = 2,
.sync = 0,
.vmode = FB_VMODE_NONINTERLACED,
.flag = 0,
};
static struct imx_epdc_fb_mode panel_modes[] = {
{
{
&es133ut2mode, /* struct fb_videomode *mode */
4, /* vscan_holdoff */
10, /* sdoed_width */
20, /* sdoed_delay */
10, /* sdoez_width */
20, /* sdoez_delay */
524, /* GDCLK_HP */
327, /* GDSP_OFF */
0, /* GDOE_OFF */
19, /* gdclk_offs */
1, /* num_ce */
},
Instead if I upload to /lib/firmware/imx/epdc the fw file received by local NXP FAE "320_R118_AD5B01_ED133UT2C1_TC.fw"
(size 1023734 bytes) and I set the parameters of the mxc_epdc_v2_fb.c file following the community.nxp.com/thread/457285 always get all the problems described above:
-At the boot the edpc display is cleared but the splash image is not drawn
-the splash image is drawn the first time I run the epdc test program or my epdc program
-....
Here the not working set of mxc_epdc_v2_fb.c file:
static struct fb_videomode es133ut2mode = {
.name="ES133UT2",
.refresh=75,
.xres=1600,
.yres=1200,
.pixclock=80000000,
.left_margin=20,
.right_margin=56,
.upper_margin=4,
.lower_margin=7,
.hsync_len=4,
.vsync_len=1,
.sync=0,
.vmode=FB_VMODE_NONINTERLACED,
.flag=0,
};
static struct imx_epdc_fb_mode panel_modes[] = {
{
&es133ut2mode, /* struct fb_videomode *mode */
4, /* vscan_holdoff */
10, /* sdoed_width */
20, /* sdoed_delay */
10, /* sdoez_width */
20, /* sdoez_delay */
796, /* GDCLK_HP */
481, /* GDSP_OFF */
0, /* GDOE_OFF */
39, /* gdclk_offs */
1, /* num_ce */
},
...
I modified the num_ce parameter from 1 to 2,3.. but I didn't see any improvement.
It could not be that the Firmware "320_R118_AD5B01_ED133UT2C1_TC.fw" was only tested with the A9 imx6 and not with A7of imx7D?
Best Regards,
Roberto Pozzi
Hello Roberto Pozzi,
Did you also change the structure per the parameters of the EPDC?
I’m investigating if it would make sense to double check the parsed waveform just in case, as it seems odd that the display works mostly well with the wrong waveform. Perhaps we can parse the original waveform again. There could
be also a problem of voltages but given the symptoms I would think it may be related to timing.
I’ll let you know as soon as I have more information.
Regards,