i.MX7D DDR3 address / command termination

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7D DDR3 address / command termination

Jump to solution
1,336 Views
davidwhitehouse
Contributor I

Hi,

I'm looking at the i.MX7D SABRE design and the IMX7DSHDG DDR recommendations in section 3.5 - the IMX7DSHDG shows VTT termination on the address and command pins but the SABRE design has nothing. What are the rules on running unterminated? If the lengths in IMX7DSHDG Table 20 are met are the traces + rise times short enough to not worry? Some words in the IMX7DSHDG on this would be very helpful - this is very fundamental

Kind regards,

Dave

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,198 Views
art
NXP Employee
NXP Employee

When the balanced T-topology routing is used (as done on the i.MX7D SABRE SD board by NXP, whose routing example is shown in the Hardware Development Guide document), no termination is required. And, yes, the main requirement is to meet the trace length rules, listed in the Table 20.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,199 Views
art
NXP Employee
NXP Employee

When the balanced T-topology routing is used (as done on the i.MX7D SABRE SD board by NXP, whose routing example is shown in the Hardware Development Guide document), no termination is required. And, yes, the main requirement is to meet the trace length rules, listed in the Table 20.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply