Hi,
I'm trying to enable 24MHz clock output to i.MX7D CCM_CLK1_P output pin (pin id = Y2). It is going to be used as reference clock to OV5640 camera sensor module. We are using Linux Yocto environment and I would like to know if it is possible to configure this somehow in Linux device tree.
I was already able to get the clock working by hard-coding / direct register write to CCM_ANALOG_CLK_MISC0n register (address 0x30360170). When LVDS1_CLK_SEL field is set to 0x15 and LVDSCLK1_OBEN bit is set to 1, the 24MHz clock appears at CCM_CLK1_P pin.
But I would assume there is a better and cleaner approach to achieve this. Is it possible to enable 24MHz clock to this pin by making configuration changes to Linux device tree only?
I've seen the IMX7D_LVDS1_OUT_SEL and IMX7D_LVDS1_OUT_CLK clocks in imx7d-clock.h file, which could be referenced from the device tree. But I don't know how to make the necessary configuration change.
This is how the device tree entry for the OV5640 sensor looks like now, I suspect that the "clocks" entry should be changed somehow perhaps by setting it to IMX7D_LVDS1_OUT_CLK. But how can I adjust the IMX7D_LVDS1_OUT_SEL field so that 24MHz gets selected?:
ov5640_mipi: ov5640_mipi@3c {
compatible = "ovti,ov5640_mipi";
reg = <0x3c>;
clocks = <&clks IMX7D_CLK_DUMMY>;
clock-names = "csi_mclk";
csi_id = <0>;
pwn-gpios = <&gpio1 12 GPIO_ACTIVE_HIGH>;
AVDD-supply = <&vgen6_reg>;
mclk = <24000000>;
mclk_source = <0>;
port {
ov5640_mipi_ep: endpoint {
remote-endpoint = <&mipi_sensor_ep>;
};
};
};
Any advice on this? Is it possible via device tree, or do I need to handle this in code?
Best regards,
Rasmus Rahunen
解決済! 解決策の投稿を見る。
Hi Rasmus
one can check available clock options in clk-imx7d.c
linux-2.6-imx.git - Freescale i.MX Linux Tree
linux/include/dt-bindings/clock/imx7d-clock.h
use assigned-clocks, assigned-clock-parents dts properties described in clock-bindings.txt
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Rasmus
one can check available clock options in clk-imx7d.c
linux-2.6-imx.git - Freescale i.MX Linux Tree
linux/include/dt-bindings/clock/imx7d-clock.h
use assigned-clocks, assigned-clock-parents dts properties described in clock-bindings.txt
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for this advice. I managed to get it working with your help!
Here is the device tree node for the OV5640, I've highlighted the important changes in red color:
ov5640_mipi: ov5640_mipi@3c {
compatible = "ovti,ov5640_mipi";
reg = <0x3c>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_camera>;
clocks = <&clks IMX7D_LVDS1_OUT_CLK>;
clock-names = "csi_mclk";
assigned-clocks = <&clks IMX7D_LVDS1_OUT_SEL>, <&clks IMX7D_OSC_24M_CLK>;
assigned-clock-parents = <&clks IMX7D_OSC_24M_CLK>;
csi_id = <0>;
pwn-gpios = <&gpio1 12 GPIO_ACTIVE_HIGH>;
AVDD-supply = <&vgen6_reg>;
mclk = <24000000>;
mclk_source = <0>;
port {
ov5640_mipi_ep: endpoint {
remote-endpoint = <&mipi_sensor_ep>;
};
};
};
In addition I had to make one small tweak to the arch/arm/mach-imx/clk-imx7d.c file. By default it doesn't support all available clock output options that are defined in i.MX7D reference manual for the LVDS1_CLK_SEL field and I had to add a few entries to the lvds1_sel array, so that the 24MHz clock ("osc") is defined in the array index 0x15:
static const char *lvds1_sel[] = { "pll_arm_main_clk",
"pll_sys_main_clk", "pll_sys_pfd0_392m_clk", "pll_sys_pfd1_332m_clk",
"pll_sys_pfd2_270m_clk", "pll_sys_pfd3_clk", "pll_sys_pfd4_clk",
"pll_sys_pfd5_clk", "pll_sys_pfd6_clk", "pll_sys_pfd7_clk",
"pll_audio_post_div", "pll_video_post_div", "pll_enet_500m_clk",
"pll_enet_250m_clk", "pll_enet_125m_clk", "pll_enet_100m_clk",
"pll_enet_50m_clk", "pll_enet_40m_clk", "pll_enet_25m_clk",
"pll_dram_main_clk", "UNDEFINED_CLOCK", "osc" };
With these two changes, the 24MHz clock appears at the CCM_CLK1_P output pin.
Best regards,
Rasmus