i.MX7 Wi-Fi Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 Wi-Fi Support

706 Views
sourabhzunke090
Contributor I

For the Variscite iMX7 SoM, can the Wi-fi be configured to work in AP+station mode? .

ie it can act as access point and simultaneously connect to other access point.

Labels (1)
0 Kudos
Reply
1 Reply

519 Views
art
NXP Employee
NXP Employee

No, it is not possible to configure the WiFi interface of the Variscite iMX7 SoM the way you describe.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply