i.MX7 Dual unused recommended connection for PCIE_VP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 Dual unused recommended connection for PCIE_VP

Jump to solution
566 Views
m_c
Senior Contributor I

In i.MX7 Dual data sheet revision 5. 

In table 3. for PCIE_VP, User can tie these pins to ground with a 10 KΩ resistor if not using PCIe.

pastedImage_2.png

In table 5. for PCIE_VP, tie to ground.

pastedImage_3.png

Q1: Which one is recommended?

Q2: Is above recommendation apply to all i.MX7 Dual revision (1.0~1.3) or only 1.3?

Labels (1)
0 Kudos
1 Solution
458 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I confirmed that the correct recommendation is tying the PCIe voltage pins (PCIE_VP,PCIE_VP_RX,PCIE_VP_TX, PCIE_VPH,PCIE_VPH_RX,PCIE_VPH_TX, PCIE_REXT) tie to ground, as per Table 5 of the Datasheet.

It will be fixed on the next release of the documentation.Sorry for the inconvenience may cause.

Best regards

TIC

View solution in original post

0 Kudos
1 Reply
459 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I confirmed that the correct recommendation is tying the PCIe voltage pins (PCIE_VP,PCIE_VP_RX,PCIE_VP_TX, PCIE_VPH,PCIE_VPH_RX,PCIE_VPH_TX, PCIE_REXT) tie to ground, as per Table 5 of the Datasheet.

It will be fixed on the next release of the documentation.Sorry for the inconvenience may cause.

Best regards

TIC

0 Kudos