i.MX6ul efuse boot_cfg

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ul efuse boot_cfg

Jump to solution
1,445 Views
hansm_
Contributor I

Hello together,

i would like to setup my custom board, to boot from eMMC.

In uBoot I found the fuse command.

What bank/word I have to write to access the boot_cfg[1/2/4]?

In ref manual 35.3.2 Fuse Shadow Memory Footprint I see 3 times boot_cfg at addr 0x05 to 0x07.

Does that mean bank 0 word 5/6/7 for boot_cfg[1/2/4]?

If yes, are bit 0 to 7 from boot_cfg[1] are found at bank 0 word 5 bit 0 to 7?

Greetings, Hans

Labels (3)
0 Kudos
Reply
1 Solution
947 Views
Yuri
NXP Employee
NXP Employee

Hello,

  the following may be helpful Fuse API - Boundary Devices 

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
3 Replies
947 Views
hansm_
Contributor I

@ Victor & Yuri,

thanks for your reply. I found the glue between u-boot fuse command (with banks and words), the addresses in chapter 5-1 and the position in the OTP-Area.

Greetings, Hans

0 Kudos
Reply
948 Views
Yuri
NXP Employee
NXP Employee

Hello,

  the following may be helpful Fuse API - Boundary Devices 

Regards,

Yuri.

0 Kudos
Reply
947 Views
b36401
NXP Employee
NXP Employee

Please refer table 5-1 "Boot Device Select" in chapter 5 of the Reference Manual.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply