i.MX6ul ECSPI DMA conflict

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ul ECSPI DMA conflict

Jump to solution
1,504 Views
boblu
Contributor I

We are using rel_imx_4.1.15_2.1.0_ga version kernel.

And enable ecspi3/4 with spidev.

&ecspi3 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi3>;
cs-gpios = <&gpio1 20 GPIO_ACTIVE_HIGH>;
status = "okay";
fsl,spi-num-chipselects = <1>;

spi_dev0: spi@0 {
compatible = "spidev";
spi-max-frequency = <20000000>;
reg = <0>;
status = "okay";
};
};

&ecspi4 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi4>;
cs-gpios = <&gpio2 15 GPIO_ACTIVE_LOW>;
status = "okay";
fsl,spi-num-chipselects = <1>;

spi_dev1: spi@0 {
compatible = "spidev";
spi-max-frequency = <20000000>;
reg = <0>;
status = "okay";
};
};

Then tested with latest spidev_test linux/spidev_test.c at master · torvalds/linux · GitHub 

with following command line,which start spi transfer on two thread.

#!/bin/bash

./spidev_test -D /dev/spidev3.0 -s 20000000 -S 4000 -I 3000 &
./spidev_test -D /dev/spidev2.0 -s 20000000 -S 4000 -I 3000 &

Then we get something like 

rate: tx 5721.6kbps, rx 5721.6kbps
rate: tx 5728.0kbps, rx 5728.0kbps

This is kind of low compare what is claimed in datasheet 52Mbit/s.

Is this normal? 

And also I noticed the DMA is using

IMX_DMATYPE_CSPI 7

from what I found 

RE: Issues with i.MX SPI DMA transfers — Linux SPI 

IMX_DMATYPE_CSPI_SP 8

which will be faster.

Then I tried to use 8

but then there will be DMA errors

[ 34.144603] spi_master spi3: I/O Error in DMA TX:fa0
can't send spi message: Connectio[ 34.150855] spi_master spi3: failed to transfer one message from queue
n timed out
[ 36.344630] spi_master spi2: I/O Error in DMA RX:fa0
can't send spi message: Connection timed out
[ 36.354338] spi_master spi2: failed to transfer one message from queue

So I have two questions:

1. Is 5.x Mbit/s speed normal?

2. Can I use IMX_DMATYPE_CSPI_SP?

thanks.

Labels (1)
Tags (2)
0 Kudos
1 Solution
1,377 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bob

>1. Is 5.x Mbit/s speed normal?

obtaining lower speeds than described in datasheet is normal

in operating system applications. One can expect faster speeds

in baremetal tests not using operating system.

>2. Can I use IMX_DMATYPE_CSPI_SP?

one can test it and if it works fine, use in own applications.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
1,378 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bob

>1. Is 5.x Mbit/s speed normal?

obtaining lower speeds than described in datasheet is normal

in operating system applications. One can expect faster speeds

in baremetal tests not using operating system.

>2. Can I use IMX_DMATYPE_CSPI_SP?

one can test it and if it works fine, use in own applications.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,377 Views
boblu
Contributor I

OK, thanks Igor.

0 Kudos