i.MX6solo DDR3 unused pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6solo DDR3 unused pin

751件の閲覧回数
ban45
Contributor III

Hello,

I am trying to turn on the power without mounting for DDR3 selection.

Will i.MX6solo break even if DDR3 is not implemented?
Is pin processing necessary?

Is it OK to leave the pins open?

0 件の賞賛
返信
1 返信

714件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yasunori

>Will i.MX6solo break even if DDR3 is not implemented?

no


>Is pin processing necessary?

no

>Is it OK to leave the pins open?

yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信