i.MX6solo DDR3 unused pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6solo DDR3 unused pin

750 次查看
ban45
Contributor III

Hello,

I am trying to turn on the power without mounting for DDR3 selection.

Will i.MX6solo break even if DDR3 is not implemented?
Is pin processing necessary?

Is it OK to leave the pins open?

0 项奖励
回复
1 回复

713 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yasunori

>Will i.MX6solo break even if DDR3 is not implemented?

no


>Is pin processing necessary?

no

>Is it OK to leave the pins open?

yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复