i.MX6solo DDR3 unused pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6solo DDR3 unused pin

752 Views
ban45
Contributor III

Hello,

I am trying to turn on the power without mounting for DDR3 selection.

Will i.MX6solo break even if DDR3 is not implemented?
Is pin processing necessary?

Is it OK to leave the pins open?

0 Kudos
Reply
1 Reply

715 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yasunori

>Will i.MX6solo break even if DDR3 is not implemented?

no


>Is pin processing necessary?

no

>Is it OK to leave the pins open?

yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply