i.MX6UlltraLite能否外接一个phy引出一路光口

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UlltraLite能否外接一个phy引出一路光口

246 Views
airuntao
Contributor II

您好: 请问i.MX6UlltraLite能否通过外接一路phy引出一路光口。

Tags (1)
0 Kudos
Reply
1 Reply

222 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @airuntao 

Hope you are doing well.
 
Yes, you use the ethernet interface (eth1) as an optical fiber link. You can set PHY configurations and recheck your correct configurations using ethtool eth1. The ethernet interface only supports MII and RMII. Whenever a PHYter is used for conversion between two different standards, we normally have two sides - the media independent side and the media dependent side.
The media independent side is the link between the processor and the PHYter IC whereas The media dependent side is the one that interfaces the PHYter and the SFP connector.
 
Thanks and Regards,
Sanket Parekh
0 Kudos
Reply