Hello,
I have a u-boot-imx image that gets "No HAB Events" when loaded from eMMC, but gets a HAB_INV_ASSERTION error when downloaded to RAM and run by UUU via the SDP protocol.
=> hab_status
Secure boot disabled
HAB Configuration: 0xf0, HAB State: 0x66
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x00 0x91 0x00 0x00
0x00 0x00 0x02 0x58
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)
The memory it's complaining about at 0x910000 appears to contain a copy of the DCD. I'm not surprised that it's asserting, as my CSF points to 0x877ff400:
[Header]
Version = 4.1
Security Configuration = Open
Hash Algorithm = sha256
Engine = SW
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS
[Install SRK]
File = "crts/SRK_1_2_3_4_table.bin"
Source index = 0
[Install CSFK]
File = "crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"
[Authenticate CSF]
[Unlock]
Engine = SW
Features = RNG
[Install Key]
Verification index = 0
Target index = 2
File = "crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"
[Authenticate Data]
Verification index = 2
Blocks = 0x877ff400 0x0 0x75c00 "u-boot.imx"
Do I need to have a different CSF for use under UUU that includes the relocated DCD?
Thanks in advance,
Stu
解決済! 解決策の投稿を見る。
Yes, that solved the issue. Thank you!
Stu