i.MX6ULZ DDR calibration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULZ DDR calibration

864件の閲覧回数
oferausterlitz
Senior Contributor II

Hi,

I am using a i.MX6ULZ and would like to perform DDR calibration for it.

However, I don't see the i.MX6ULZ in the i.MX6/7 DDR Stress Test Tool V3.00 CPU list nor have

I found a script aid for it.

Is the i.MX6ULZ calibration same as for i.MX6ULL? i.e. selecting i.MX6ULL and using i.MX6ULL script?

Thank you for your support

ラベル(1)
0 件の賞賛
返信
1 返信

792件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello,

You are correct, there is no script aid for the i.MX6ULZ because as you already mention you can use the i.MX6ULL they shared the same Memory Controller .


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信