i.MX6ULL where to apply DDR stress test calibrations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL where to apply DDR stress test calibrations

546 Views
chadwolter
Contributor III

Hi -

We have a custom board running a i.MX6ULL with 512MB DDR3.  We are running the "DDR Stress Test (2.6.0)" tool from NXP....we are using the GUI version over USB.  My question is:  Now that I have the calibration factors generated by the tool, where do I apply them to Uboot/Linux?  We are running the uboot-rel_imx_4.9.x_1.0.0_ga and linux-rel_imx_4.9.x for Uboot and Linux respectively.  It seems to me like there should be a script file somewhere that should do this, but I cannot seem to find it in either of these packages.  please help.

thanks in advance

Chad

Labels (1)
0 Kudos
2 Replies

358 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chad

calibration coefficients may be added to uboot dcd header :

uboot/board/freescale/mx6ullevk/imximage.cfg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

358 Views
chadwolter
Contributor III

Thanks Igor-

I actually found this about an hour after I posted the question. Happy to have it confirmed

Thanks

Chad

Sent from my iPhone

0 Kudos