i.MX6ULL framebuffer broken after resume from suspend

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6ULL framebuffer broken after resume from suspend

500 次查看
tarjeiknapstad
Contributor II

On Yocto Scarthgap I am experiencing an issue with the framebuffer device not working after resuming from suspend. When resuming, the contents of the display from just before the suspend is displayed for a brief moment until the RUN bit is set in the LCD_CTRL register from the mxsfb.c device driver. This is an LCD screen in DOTCLOCK mode. This is with the linux 6.6 branch from linux-imx from the Yocto Scarthgap layers.

This used to work fine under mickledore, but now seems comlpetely broken. Any ideas what could be wrong?

0 项奖励
回复
1 回复

461 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

This created a bug in our system, developers will fix it ASAP. thanks for the catch!.

Regards

0 项奖励
回复